This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 EDMA3问题



求高手帮助:

最近调试EDMA3,进行数据搬移。但是测试过程中突然发现程序总会开在一个循环判断上,我感觉是edma3的IPR的bit 0没有被置位,也就是没有传输完成中断被探测到。这种情况在我程序里面有时会出现有时又好了,不过现在卡住了。如下为代码:

#include <stdio.h>
#include "csl_edma3.h"
#include "csl_edma3Aux.h"

CSL_TpccRegs*  gEDMACC0Regs  = (CSL_TpccRegs*)CSL_EDMA0CC_REGS;
CSL_TpccRegs*  gEDMACC1Regs  = (CSL_TpccRegs*)CSL_EDMA1CC_REGS;
CSL_TpccRegs*  gEDMACC2Regs  = (CSL_TpccRegs*)CSL_EDMA2CC_REGS;


/* Global Buffers (Source and Destination) for PING-PONG */
Uint8 srcBuff1[512];
Uint8 dstBuff1[512];
CSL_Edma3Handle                 hModule;
CSL_Edma3Obj                    edmaObj;
CSL_Edma3ParamHandle            hParamPing;
//CSL_Edma3ParamHandle            hParamPong;
CSL_Edma3ChannelObj             chObj;
CSL_Edma3CmdIntr                regionIntr;
CSL_Edma3ChannelHandle          hChannel;
CSL_Edma3ParamSetup             myParamSetup;
CSL_Edma3Context                context;
CSL_Edma3ChannelAttr            chAttr;
CSL_Status                      status;

static Int32 edma_ping_pong_xfer_gbl_region ()
{   

   


 Uint8 channelNum=0;
 Uint8 instNum = 1;

    /* Start the EDMA PING-PONG test over the Global Region. */
    printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d...\n", instNum, channelNum);
  
 
    /* Module initialization */
    CSL_edma3Init(&context);
   
   
    /* Open the EDMA Module using the provided instance number */
    hModule = CSL_edma3Open(&edmaObj, instNum, NULL, &status);
   

    /* Channel open */
    chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;
    chAttr.chaNum    = channelNum;
    hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);
   
 
    /* Change Channel Default queue setup from 0 to 3  */
    CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_0);
   

    /* Map the DMA Channel to PARAM Block 2. */
    CSL_edma3MapDMAChannelToParamBlock (hModule, channelNum, 0);
   
    /* Obtain a handle to parameter set 2 */
    hParamPing = CSL_edma3GetParamHandle(hChannel, 0, &status);
   
 
    /* Obtain a handle to parameter set 1 */
 //   hParamPong = CSL_edma3GetParamHandle(hChannel, 1, &status);
   
 
    /* Setup the parameter entry parameters (Ping buffer) */
//    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
                                             CSL_EDMA3_TCCH_DIS, \
                                             CSL_EDMA3_ITCINT_DIS, \
                                             CSL_EDMA3_TCINT_EN, \
                                             0, CSL_EDMA3_TCC_NORMAL,\
                                             CSL_EDMA3_FIFOWIDTH_NONE, \
                                             CSL_EDMA3_STATIC_DIS, \
                                             CSL_EDMA3_SYNC_A, \
                                             CSL_EDMA3_ADDRMODE_INCR, \
                                             CSL_EDMA3_ADDRMODE_INCR );
    myParamSetup.option = 0x00100008;
 myParamSetup.srcAddr = (Uint32)srcBuff1;
 myParamSetup.aCntbCnt = 0x00010200;
 myParamSetup.dstAddr = (Uint32)dstBuff1;
 myParamSetup.srcDstBidx = 0x0;
 myParamSetup.linkBcntrld = 0x0000ffff;
 myParamSetup.srcDstCidx = 0x0;
 myParamSetup.cCnt = 0x00000001;

    /* Ping setup */
    CSL_edma3ParamSetup(hParamPing,&myParamSetup);
  
    /* Interrupt enable (Bits 0-1)  for the global region interrupts */
    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
    regionIntr.intr   = 0x3;
    regionIntr.intrh  = 0x0000;
    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&regionIntr);

    /* Trigger channel */
    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
    regionIntr.intr   = 0;
    regionIntr.intrh  = 0;

    /* Poll on IPR bit 0 */
    do {
        CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x1));

    /* Clear the pending bit */
    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&regionIntr);

        
    /* Close channel */
    CSL_edma3ChannelClose(hChannel);
   
 
    /* Close EDMA module */
    CSL_edma3Close(hModule) ;
   
 return 0;

   }
 


void main (void)
{

    Uint32 loopIndex;
    
    printf ("**************************************************\n");
    printf ("******************* EDMA Testing *****************\n");
    printf ("**************************************************\n");

    for (loopIndex = 0; loopIndex < 512; loopIndex++)
    {
        srcBuff1[loopIndex] = 0xff;

        dstBuff1[loopIndex] = 0;
     }
 
    edma_ping_pong_xfer_gbl_region ();
    for(loopIndex=0;loopIndex<512;loopIndex++)
     {
      printf("dstBuff1[loopIndex] = %d  %d\n",loopIndex,dstBuff1[loopIndex]);

     }
    printf ("**************************************************\n");
    printf ("************* EDMA Testing Successful ************\n");
    printf ("**************************************************\n");
  
    return;
}

 

开住的地方在:    /* Poll on IPR bit 0 */
    do {
        CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x1));

哪位遇到过这种情况,求解答!另外想请教下这段代码是什么意思:

   1、 regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
  /2、 regionIntr.intr   = 0;
   /3、regionIntr.intrh  = 0;

主要是2和3,。

  • regionIntr是一个结构体,他可以根据函数调用参数的不同赋予不同的含义,在这里是IPR寄存器的值,在读取IPR值之前清0。

    你的代码我在6678 sim上可以测试通过,不知你测试的环境?

  • 我的测试环境是CCS5.1,TI的EVM6678L开发板,刚才测了下,还是时好时坏,这个IPR值如果探测到传输中断的话应该是自动置1的吧?总感觉什么地方导致传输中断没被探测到或者没发生传输.。另外,不同的IPR值可以代表不同的通道?是这样的吗?

  • 我也遇到同样的问题,我查看了所有的寄存器的配置和错误诊断寄存器,都没有发现异常的地方.

  • 我也遇到了一样的问题,不知道能否帮忙解答一下,测试环境是ccs5.2 evmc6678le Rev 3B。另外请问在使用EDMA进行pingpong的时候需要开启中断吗?如果测试成功的话dstBuff中的数据应该和srcBuff一样吧

  • 不要用CSL操作EDMA3,这个不是thread safe的,换LLD

  • 我也遇到这个问题了,我觉得CSL操作应该没错,这个edma测试是csl里的例程!没有产生中断的原因是CPU触发方式的edma根本没有进行数据搬运,ACNT一直是256,BCNT=CCNT=1,所以根本没法产生中断!

    另外,即使进行数据搬运了这个代码写的也有问题,因为它只触发了一次edma事件,所以只能搬运一次,因为是A-SYNC方式的搬运,所以需要256(ACNT)触发才能产生中断(opt中只打开了最后一次搬运的中断,即TCINTEN=1)。

    请问不能进行数据搬运的原因是什么,希望高手能给指点!谢谢,谢谢!

  • 你好,请问这个问题你解决了吗,我现在也遇到这个问题了!这个代码确实有问题,但不应该影响第一次的数据搬运,为什么根本没有触发edma事件啊?