您好工程师,我目前正在使用6678进行调试
我们设计的板卡DDR3已经可以正常初始化和读写,但是对于与DDR3相连的EMIF64位总线还有一些疑问
1.首先当内核需要对DDR3进行操纵肯定会使用EMIF64总线,但是如果当此时采用EDMA对DDR3也进行数据操作,那么EMIF64总线是否支持同时操作,会不会出现总线冲突,如果冲突那么采取什么措施规避冲突
2.由外部SRIO接口如果向6678的外挂的DDR3写数据,那么数据传输也会占用EMIF64位总线,那么如果同时EDMA操作需要读取DDR3的另一地址空间的数据,EMIF64位总线会冲突吗?