This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358 MMC1接口挂载EMMC存储器时VDDSHV1的输入电压疑问

Other Parts Discussed in Thread: AM3358

大家好,我在设计AM3358核心板的时候遇到了一个疑问,我的EMMC存储芯片挂在MMC1接口上,电压是1.8V,但是参考设计上是连接到VAUX2(3.3V),我需要将VDDSHV1换到1.8V吗,但是如果是连接到1.8V的话其它连接到VDDSHV1的IO是不是也变成1.8V了?

另外,我还想知道VDDSHVx的输入电压是否是和所控制的IO电压有关系?也就是说IO口的电压是不是由所对应的VDDSHVx决定的呢?

我的PMU选择的是TPS65910A31A1,根据手册的说明BOOT1连接到VRTC,BOOT0连接到GND,各路输出电压和时序由EEPROM决定,那么在这种情况下我可不可以单独修改某个输出的电压呢?如果可以,我应该如何修改?

再次感谢大家能够耐心解答我的问题,谢谢!