This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6674和66AK2L06的功耗估算问题

Other Parts Discussed in Thread: TMS320C6674, TMS320C6678

您好,我现在的工作是将之前板子上的TMS320C6674更换为66AK2L06,以便在板子上可以跑Linux,在这过程中:

使用sprm559a对C6674进行功耗,在设定完资源使用后,发现壳温为0度时,6674的功耗为3876.94mW;壳温为70度时,6674的功耗为5911.62mW,这里相差了近2W。

而使用sprm656对66AK2L06进行功耗估算时,在设定完相同的外设资源使用率时(和C6674相比,仅ARM核设定不一致),壳温为0度时的功耗为6.356W,壳温为70度时的功耗为7.034W,这里只相差了0.7W。

我想问一下:

1.C6674和66AK2L06这两颗芯片,由于壳温(外界温度)不相同,C6674前后估算出的功耗差了2W,而66AK2L06前后估算出的功耗只差了0.7W。这是正确的吗?

2.由于C6674和66AK2L06使用的外设资源相同,仅仅是66AK2L06比C6674多运行两个ARM核跑Linux,这两个芯片的实际运行功耗应该是比较接近的吧(都是4个C66x核,而且66AK2L06属于28nm制程芯片,功耗应该较C6674有所优化)。我可以参考我们上一版中C6674的功耗来估计66AK2L06的功耗吗?(我看随着壳温的增加,C6674的功耗和66AK2L06的功耗会相接近)

3.如果可以用C6674的功耗来预计66AK2L06的功耗,那么之前C6674是采用的被动散热,是否可以在66AK2L06上继续沿用这种被动散热呢?

4.66AK2L06芯片上的VDDCMON(引脚号为K10)是否可以按《SPRS930》中第41页说的直接连接至CVDD(我看了一个帖子说是CVDD,不是CVDDS)?而不需要按评估板上的接法,连接至CVDD电源的SS脚。

这是我的疑问,希望能得到您的解答。非常感谢!