This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 emif例程



做k1_stk_v1.1 emif 例程时 编译后出现"../src/EMIF_main.c", line 125: error #20: identifier "CSLSIZE_PSC_PD_ALWAYSON" is undefined   

  

/****************************************************************************\
 *           Copyright (C) 2012 Texas Instruments Incorporated.             *
 *                           All Rights Reserved                            *
 *                                                                          *
 * GENERAL DISCLAIMER                                                       *
 * ------------------                                                       *
 * All software and related documentation is provided "AS IS" and without   *
 * warranty or support of any kind and Texas Instruments expressly disclaims*
 * all other warranties, express or implied, including, but not limited to, *
 * the implied warranties of merchantability and fitness for a particular   *
 * purpose.  Under no circumstances shall Texas Instruments be liable for   *
 * any incidental, special or consequential damages that result from the    *
 * use or inability to use the software or related documentation, even if   *
 * Texas Instruments has been advised of the liability.                     *
 ****************************************************************************
This example shows EMIF operations:
1. NAND FLASH test, Verified on NAND512R3A2DZA6E on Shannon EVM,
                               MT29F1G08ABBDAHC on Appleton EVM.
2. NOR FLASH test, Verified on JS28F256M29EW on a customer's board.
 ****************************************************************************
 * Created by :                                                             *
 *            Brighton Feng                                                 *
 *            Texas Instruments                                             *
 *            Jan 5, 2012                                                 *
***************************************************************************/
#include <stdio.h>
#include <string.h>
#include "KeyStone_common.h"
#include "Keystone_DDR_Init.h"
#include "KeyStone_EMIF16_init.h"
#include "EMIF_NOR_FLASH_test.h"
#include "EMIF_NAND_FLASH_test.h"
/*select between NAND FLASH or NOR FLASH test*/
#define NAND_FLASH_TEST  1
#define FLASH_TEST_BUFFER_SIZE  (1*1024*1024)
#pragma DATA_SECTION(testBuf,".far:testBuf")
Uint8 testBuf[FLASH_TEST_BUFFER_SIZE];
EMIF16_CE_Config gNorCeCfg; /*the configuration for the CE of NOR FLASH*/
EMIF16_CE_Config gNandCeCfg;/*the configuration for the CE of NAND FLASH*/
EMIF16_Config gEmif16Cfg;
void EMIF_init()
{
 memset(&gNorCeCfg, 0, sizeof(gNorCeCfg));
 memset(&gNandCeCfg, 0, sizeof(gNandCeCfg));
 memset(&gEmif16Cfg, 0, sizeof(gEmif16Cfg));
 
 /*configuraiton for the CE of NOR FLASH*/
 gNorCeCfg.busWidth= EMIF_BUS_16BIT;
 gNorCeCfg.opMode  = NOR_ASRAM_MODE;
 gNorCeCfg.strobeMode = SS_STROBE; 
 gNorCeCfg.waitMode = EMIF_WAIT_NONE;
 gNorCeCfg.wrSetup = CSL_EMIF16_A0CR_WSETUP_RESETVAL;         
 gNorCeCfg.wrStrobe = CSL_EMIF16_A0CR_WSTROBE_RESETVAL;        
 gNorCeCfg.wrHold= CSL_EMIF16_A0CR_WHOLD_RESETVAL;           
 gNorCeCfg.rdSetup= CSL_EMIF16_A0CR_RSETUP_RESETVAL;          
 gNorCeCfg.rdStrobe= CSL_EMIF16_A0CR_RSTROBE_RESETVAL;         
 gNorCeCfg.rdHold= CSL_EMIF16_A0CR_RHOLD_RESETVAL;           
 gNorCeCfg.turnAroundCycles= CSL_EMIF16_A0CR_TA_RESETVAL; 
 gNorCeCfg.nor_pg_Cfg= NULL;       
 /*configuraiton for the CE of NAND FLASH*/
 gNandCeCfg.busWidth= EMIF_BUS_8BIT;
 gNandCeCfg.opMode  = NAND_MODE;
 gNandCeCfg.strobeMode = SS_STROBE; 
 gNandCeCfg.waitMode = EMIF_WAIT_NONE;
 /*timing configuration for NAND512R3A2DZA6E*/
#if 1
 gNandCeCfg.wrSetup = 1;//CSL_EMIF16_A0CR_WSETUP_RESETVAL,         
 gNandCeCfg.wrStrobe = 4;//CSL_EMIF16_A0CR_WSTROBE_RESETVAL,        
 gNandCeCfg.wrHold= 5;//CSL_EMIF16_A0CR_WHOLD_RESETVAL,           
 gNandCeCfg.rdSetup= 1;//CSL_EMIF16_A0CR_RSETUP_RESETVAL          
 gNandCeCfg.rdStrobe= 7;//CSL_EMIF16_A0CR_RSTROBE_RESETVAL         
 gNandCeCfg.rdHold= 2;//CSL_EMIF16_A0CR_RHOLD_RESETVAL           
#else
 gNandCeCfg.wrSetup = CSL_EMIF16_A0CR_WSETUP_RESETVAL;         
 gNandCeCfg.wrStrobe = CSL_EMIF16_A0CR_WSTROBE_RESETVAL;        
 gNandCeCfg.wrHold= CSL_EMIF16_A0CR_WHOLD_RESETVAL;           
 gNandCeCfg.rdSetup= CSL_EMIF16_A0CR_RSETUP_RESETVAL;          
 gNandCeCfg.rdStrobe= CSL_EMIF16_A0CR_RSTROBE_RESETVAL;        
 gNandCeCfg.rdHold= CSL_EMIF16_A0CR_RHOLD_RESETVAL;           
#endif
 gNandCeCfg.turnAroundCycles= CSL_EMIF16_A0CR_TA_RESETVAL; 
 gNandCeCfg.nor_pg_Cfg= NULL;       
#if NAND_FLASH_TEST
 gEmif16Cfg.ceCfg[0] = &gNandCeCfg;
#else
 gEmif16Cfg.ceCfg[0] = &gNorCeCfg;
#endif
 gEmif16Cfg.wait0Polarity= EMIF_LOW_WAIT;
 gEmif16Cfg.wait1Polarity= EMIF_LOW_WAIT;
 gEmif16Cfg.maxWait = CSL_EMIF16_AWCCR_MAXEXTWAIT_RESETVAL;
 
 KeyStone_EMIF16_init(&gEmif16Cfg);
}
void main()
{
 /*enable TSC, memory protection interrupts, EDC for internal RAM;
    clear cache; protect L1 as cache*/
 KeyStone_common_CPU_init();
 /*print device information.
 Enable memory protection interrupts, EDC for MSMC RAM*/
 KeyStone_common_device_init();
 //enable exception handling
 KeyStone_Exception_cfg(TRUE);
    // System init
    CACHE_setL1PSize(CACHE_L1_32KCACHE);
    CACHE_setL1DSize(CACHE_L1_32KCACHE);
    CACHE_setL2Size(CACHE_128KCACHE);
 if(C6678_EVM==gDSP_board_type)
 {
  //DSP core speed: 100*10/1=1000MHz
  KeyStone_main_PLL_init(100, 10, 1);
  //On Shannon, EMIF belong to clock domain 3 which need be enabled
  KeyStone_enable_PSC_module(CSLSIZE_PSC_PD_ALWAYSON, 3);
 }
 else if(TCI6614_EVM==gDSP_board_type)
 {
  //DSP core speed: 122.88*236/29= 999.9889655MHz
  KeyStone_main_PLL_init(122.88, 236, 29);
 }
 else
 {
  puts("Unknown DSP board type!");
  return;
 }
 //DDR init 66.66667*20/1= 1333
 KeyStone_DDR_init (66.66667, 20, 1, NULL);
 EMIF_init();
#if NAND_FLASH_TEST
 NAND_FLASH_test((Uint32)testBuf, FLASH_TEST_BUFFER_SIZE);
#else
 NOR_FLASH_test((Uint32)testBuf, FLASH_TEST_BUFFER_);
#endif
 puts("FLASH test complete.");
}