我已经将tftp服务器ip地址设置为192.168.1.210,但是在使用tftp下载镜像时怎么地址还是192.168.1.1?
=> printenv serverip serverip=192.168.1.210 => tftp 0x82000000 zImage link up on port 0, speed 100, full duplex Using cpsw device TFTP from server 192.168.1.1; our IP address is 192.168.1.203 Filename 'zImage'. Load address: 0x82000000 Loading: T T T T T T T T T T T T T T T T T T T T Retry count exceeded; starting again