This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368用gstreamer录制1280*1024,25hz的视频4h的问题



大家好

我用gstreamer录制1280*1024,25hz的视频 连续录制4小时,后停止录像,这段录像回放是正常的,但是当我重新在录像时发现录像一会后,录像程序就死了,同时功耗也降下来了,请问各位知道是什么原因吗?  

我觉得是我的bootargs的问题,但是我你不知道具体是哪的问题。

我的bootargs如下:

setenv bootargs "console=ttyS0,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off mem=64M davinci_enc_mngr.ch0_mode=720P-60 davinci_enc_mngr.ch0_output=LCD vpfe_capture.cont_bufoffset=13631488 vpfe_capture.cont_bufsize=12582912 video=davincifb:vid0=OFF:vid1=OFF:osd0=1280*1024*16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=0"

请问各位以及TI的专家,能给些建议吗?

谢谢