This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCP3D_C对应区域的初始化问题



pdk中只提供了tcp_A和tcp_B的例程。

根据例程修改的emulator初始化函数为:

FUNC_STATE enable_tcp3d (Tcp3d_Region_Sel region_num)
{
#ifndef SIMULATOR_SUPPORT
    /* TCP3D power domain is turned OFF by default.
     * It needs to be turned on before doing any TCP3D device register access.
     * This is not required for the simulator. */
 UINT CSL_PSC_PD_TCP3D,CSL_PSC_LPSC_TCP3D;
 if ((int)region_num == 0)
 {
  CSL_PSC_PD_TCP3D = CSL_PSC_PD_TCP3D_A;
     CSL_PSC_LPSC_TCP3D = CSL_PSC_LPSC_TCP3D_A;
 }
 else if((int)region_num == 1)
 {
  CSL_PSC_PD_TCP3D = CSL_PSC_PD_TCP3D_B;
     CSL_PSC_LPSC_TCP3D = CSL_PSC_LPSC_TCP3D_B;
 }
 else if(((int)region_num == 2)) //这里有问题
 {
  CSL_PSC_PD_TCP3D = CSL_PSC_PD_BCP_FFTC_C_TCP3D_C;
     CSL_PSC_LPSC_TCP3D = CSL_PSC_LPSC_BCP_FFTC_C_TCP3D_C;
 }
    /* Set TCP3D Power domain to ON */
    CSL_PSC_enablePowerDomain (CSL_PSC_PD_TCP3D);

    /* Enable the clocks too for TCP3D */
    CSL_PSC_setModuleNextState (CSL_PSC_LPSC_TCP3D, PSC_MODSTATE_ENABLE);

    /* Start the state transition */
    CSL_PSC_startStateTransition (CSL_PSC_PD_TCP3D);

    /* Wait until the state transition process is completed. */
    while (!CSL_PSC_isStateTransitionDone (CSL_PSC_PD_TCP3D));

..............

}

 

对于tcp_A,我们可以使用CSL_PSC_PD_TCP3D_A和CSL_PSC_LPSC_TCP3D_A;对于tcp_B,同样有对应的Definitions。

可是对于TCP3D_C, 却没有对应CSL_PSC_PD_TCP3D 、CSL_PSC_LPSC_TCP3D的Definitions,导致tcp3d_C对应的区域0x35020000 和0x35600000无法访问。

请教专家:

                     tcp3d_C是这么用的吗?如果是的,那该如何进行初始化呢?

  • 你用的没错,TCP3D_C就是用的CSL_PSC_PD_BCP_FFTC_C_TCP3D_C和CSL_PSC_LPSC_BCP_FFTC_C_TCP3D_C。请详细描述你遇到的问题。

  • Andy Yin1,您好,

        我在尝试使用TCP3D的时候发现,Void allInit(Void)函数中完全没有关于TCP3D_C的初始化,在TCP3D的用户指南中也未区别A B C 来说明,请问C与AB有很大的区别吗?我该去哪里查看相关资料?我知道6670的数据手册中有一些A B C 参数的说明。

       非常感谢

  • 三个TCP3D的功能及使用没有任何区别,只是其隶属不同的电源控制器PSC,并且每个TCP3D各自的寄存器地址不一样。你直接看TCP3D手册了解其使用,看6670 data manual可以看到各个TCP3D的基地址及其对应的PSC,可以同时参考6670 csl r_ device.h中对各地址及PSC的宏定义。