This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all,
I use the SDK 3.0.5 and turn on the fast boot function in my TDA2x board.
I used the core-tex A15 u-boot to load the IPU/DSP firmware and boot them.
After the Linux kernel boot finished, I get the message
2.713536 s: ***** IPU2 Firmware build time 19:56:30 Jun 18 2019
2.713688 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 16393 Hz>
2.716891 s: SYSTEM: System Common Init in progress !!!
The IPU2 frequency is too slow, but the other core frequency the correct
2.589123 s: ***** DSP1 Firmware build time 19:54:43 Jun 18 2019
2.589214 s: *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 600000000 Hz>
2.589489 s: SYSTEM: System Common Init in progress !!!
how can I change the IPU2 frequency to correct setting?
*** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>