This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 支持500万像素的resize吗?



display 输出只有一部分 想开一条捕获流但是发现resize都被占用!该如何办?

  • VPFE缺省下是用Resize做422-420转换的,不然无法获得编码器需要的数据格式,你是想用500万采集,然后通过Resize成Display支持的720P或者1080I/1080P么?可以尝试用Resize的另一个通道做一个副码流,不过不保证Resize能支持一路500万RGB-YUV420,在支持一路500万RGB-Resize720P

  • 500MP已经超过了IPIPE的line buffer限制,500MP采集要过两次IPIPE, IPNC 2.6已经实现500MP的抓拍功能,请参考IPNC 2.6的代码,谢谢

  • 您好,Tuff Li 我现在用过的是DVSDK4.02 来做DM368 ,采集500W sensor ,分辨率是2432X2048,但是DM368 one-shot模式,只能采集宽度为2176的像素,图像宽度超出的部分,也就是2432-2176个像素会变花,请问用DVSDK 4.02怎么缩放2次IPIPE实现2432X2048的图像采集呢。我也看了APPRO 2.6 关于2592X1920分辨率的缩放,不是很清楚,希望Tuff Li 指点一下,我的邮箱是:niuliwei2012@163.com 谢谢了。