你好,请问下,GPS模块直连dm8148的串口2,没有生成对应的设备节点,我无法读取节点来获取数据;请问下是啥原因?(串口驱动不是自带并已经实现的么? 应该不需要改吧)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问下,GPS模块直连dm8148的串口2,没有生成对应的设备节点,我无法读取节点来获取数据;请问下是啥原因?(串口驱动不是自带并已经实现的么? 应该不需要改吧)
你好 pinmux已经正确配置了 我将串口4的rx和tx短接后,可以发送和接收数据 但是我将串口2的rx和tx短接后,只能发送,不能接收到数据(其中串口2和串口4的pinmux都已经正确配置了)
你好,已经检测了 没有将其它的引脚配置uart2的功能,现在不知道该怎么办了
你好,
请问你是否有把可以支持UART2的引脚的pinmux寄存器都读出来,排查一下?
硬件连接上也排查一下。
你好,
请参考DM8148数据手册(http://www.ti.com/lit/ds/symlink/tms320dm8148.pdf)160~169页,里面有多个PINCNTL寄存器可以配置UART2相关引脚,请都读出来检查一下。
你好 我知道哪些引脚可以配置uart2,但是读寄存器我不知道怎么操作,或者是用什么命令来读寄存器
你好,所有能配置成uart2的引脚的寄存器都读取了,没有重复配置uart2,硬件连接上需要注意什么? 同样的电路设计,其它几个uart口没问题;;;现在完全不知道怎么做了?