This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助!OMAPL137 USB连接U盘的问题!



我准备通过开发板(OMAPL137)的USB接口通过一个OTG线连接一个U盘,进行数据的存入,将usb设置成主机模式,请问我这样的构想可行吗?

在实验中发现PHY总是初始化不成功,时钟、电源、PLL锁存这几个方面出现了问题,时钟我通过USB_REFCLKIN给48MHZ;电源我不太清楚,直接连上U盘,U盘显示有电状态;PLL我没有管,我觉着是PLL自动锁存。  在CFGCHIP2寄存器中,我通过设置最终读取的值为:0x00011173,第16位如果是1,就显示PHY初始化成功了,但我一些无法成功,请问我还用怎么的额外设置吗??或者说电源、时钟、PLL锁存方面出现了错误?

刚开始研究DSP,求助!

  • 可以实现。请下载最新的SDK。
    www.ti.com/.../processor-sdk-omapl137
    仔细阅读以下文档,pdk里有相关例程USB host Mass Storage Class。
    software-dl.ti.com/.../index_device_drv.html
    USB host Mass Storage Class
    In this mode, the USB instance will act as a USB host communicating with a USB device that supports Mass Storage Class function (USB thumb drive or a small USB hard drive). The demo example code utilizes a shell interface via the EVM via UART for interaction with the example. The shell provides some basic commands to manipulate the content of the attached USB disk drive.
  • 谢谢您的帮助!
    我已经下载链接中的SDK文件,并且阅读了相关文档,还有几点困惑还需向您请教:
    1、SDK文件下载完后如何打开使用?我电脑是win7/32位的CCS3.3和5.5,目前打不开,是系统原因吗?
    2、我开发板的是OMAPL137-KB,包括DSPC6747和ARM双系统,通过C6747可以完成吗?还是我的理解出现了问题?
    麻烦您了,我可能储备知识太少,希望您能解答!