This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 sgmii已经link上了,但是与pc机ping不通

我的程序是在helloworld的例程上稍微改动了一下,运行时提示:

[C66xx_0]

QMSS successfully initialized

CPPI successfully initialized

PA successfully initialized

TCP/IP Stack 'Hello World!' Application

TCP/IP Stack 'Hello World!' Application

PASS successfully initialized

Ethernet subsystem successfully initialized

Ethernet eventId : 48 and vectId (Interrupt) : 7

Registration of the EMAC Successful, waiting for link up ..

Network Added: If-1:192.168.118.212

我使用的是SGMII1 PHY模式,查看SGMII_CONTROL  STATUS  MR_ADV_ABILITY三个寄存器值为:00000001 0000003D 00009801,我看了一下这几个寄存器的值也应该正确,但是我和PC机 就是ping不通,请问大家有遇见这种情况的吗?怎么解决的?