This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dn6467 添加算法lib库出错



在做个项目,其中涉及到davinci集成ccs下编译的lib库,我是在ti提供的scale例子下进行的修改。可以实现arm与dsp的简单通信,为了测试集成算法的情况,我需要添加codecl算法库。我在server目录下的link.cmd文件下进行添加库,我做了。但是其他的bld,xdc等文件我没改动。现在的问题是只要我调用库中的函数,集成codec server就出错。我估计是我配置文件的问题,再一个是不是scale这个例子不能添加自己的库?已经困扰很多天了,一直无法解决,求解.........

undefined                        first referenced
 symbol                              in file
---------                        ----------------
_InitTest                        /mnt/sda3/wangyanlong_extend/dvsdk_1_40_02_33/dm6467_dvsdk_combos_1_17/packages/ti/sdo/codecs/scale/lib/scale_ti.a64P
>>   error: relocation overflow occurred at address 0x0000004c in section
            '.text' of input file 'ImgProcTest.o64P
            (/mnt/sda3/wangyanlong_extend/dvsdk_1_40_02_33/dm6467_dvsdk_combos_1_17/packages/ti/sdo/codecs/scale/lib/scale_ti.a64P)'.  The 29-bit PC-relative displacement 471294248 at this location is too large to fit into the 21-bit PC-Relative field; the destination address is too far away from the instruction.