This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368安装gst-plugins-base的问题

我的系统上层安装过gstreamer   但是缺少编码音频所需要的alsasrc   查阅资料后发现需要安装gst-plugins-base (我不知道之前是否有安装过gst-plugins-base)

当我下载了源码并执行./configure    报了一下错误

lloc.h presence... yes
checking for malloc.h... yes
Package libxml-2.0 was not found in the pkg-config search path.
Perhaps you should add the directory containing `libxml-2.0.pc'
to the PKG_CONFIG_PATH environment variable
No package 'libxml-2.0' found
checking sys/socket.h usability... yes
checking sys/socket.h presence... yes
checking for sys/socket.h... yes
checking winsock2.h usability... no
checking winsock2.h presence... no
checking for winsock2.h... no
checking for hstrerror... yes
checking process.h usability... no
checking process.h presence... no
checking for process.h... no
checking for sys/types.h... (cached) yes
checking sys/wait.h usability... yes
checking sys/wait.h presence... yes
checking for sys/wait.h... yes
checking for sys/stat.h... (cached) yes
checking for stdint types... stdint.h (shortcircuit)
make use of stdint.h in _stdint.h (assuming C99 compatible system)
checking for localtime_r... yes
checking for gmtime_r... yes
checking for FIONREAD in sys/ioctl.h... yes
checking for _LARGEFILE_SOURCE value needed for large files... no
checking for lrint... yes
checking for lrintf... yes
checking whether gcc implements __PRETTY_FUNCTION__... yes
checking whether gcc implements __FUNCTION__... yes
checking whether gcc implements __func__... yes
checking for socket... yes
checking for gethostbyname... yes
checking for GLIB... yes
checking for ORC... no
checking for GST... no
no
configure: No package 'gstreamer-0.10' found
configure: error: no gstreamer-0.10 >= 0.10.30 (GStreamer) found

请问 各位知道这是什么原因吗   我的系统里安装了gstreamer-0.10   并且一直在用   是需要修改什么环境变量吗

谢谢