This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748读写NorFlash S29GL256S10问题



S29GL256S10 是16位NorFlash,挂在CS2,C6748的BA1连接NorFlash的A0,C6748的A0连接NorFlash的A1,依次类推。NorFlash的驱动是在C6713中长期使用的,移植到C6748中只改了EMIF的的配置,时钟速率同为40MHz,Stepup/Strobe/Hold时间设置与原来相同,EMIF已开启并配置了pinmux

现象描述:1)能读取NorFlash 的 Manufacture ID 和 Device ID(硬件连接应该正确)

                  2)擦除操作后状态显示擦除成功(方法是:Polling DQ7等bit)

                  3)写入操作后状态显示写入成功,但回读数据全是0xFFFF

                  4)用CCS6.1.1的Memory Browser看到的数据和程序读出的一致(0xFFFF),有个异常现象是读取完成后发送“写入缓冲区终止复位指令”,Memory                                   Browser看到的数据编程了0x008A和0x00CA等重复数值

                 “写入缓冲区终止复位指令”:

                *(volatile Uint16 *)(FLASH_addr555) = 0xAA;
                *(volatile Uint16 *)(FLASH_addr2aa) = 0x55;
                *(volatile Uint16 *)(FLASH_addr555) = 0xF0;

麻烦各位看看有无拍错思路,卡了两天了,感谢