This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 NDK与MessageQ一起工作时,ping延迟较大



环境:DSP6678、mcsdk_2_01_02_06、ndk_2_21_02_43、ipc_1_24_03_32

移植的是官方提供的NDK和MessageQ程序,Core0上移植了NDK、MessageQ;Core1、Core2移植了MessageQ。

运行过程是PC主动ping Core0,同时Core0、Core1、Core 2通过MessageQ相互发消息。程序正常运行。

问题现象:

1:当使用messageQ时,ping会出现几十毫秒的延迟;

2:当不使用messageQ发消息时,ping延迟都在1ms以内;

请问下,这会是什么问题导致的??,谢谢