以下是从multi_core_EMAC_boot\Shannon_boot_notes摘录的:
1.1 EMAC boot by PC
1.1.1 准备工作
- 正确配置EVM板的拨码开关。配置正确以后PC就能收到EVM发出的BOOTP包(3s周期)
EVM板型号是TMDXEVM6678LE Rev1.0
The DIP switch setting for C6678 EVM is:
SW3(pin1, pin2, pin3, pin4): off, on, off, on
SW4(pin1, pin2, pin3, pin4): on, on, on, off
SW5(pin1, pin2, pin3, pin4): on, on, off, off
SW6(pin1, pin2, pin3, pin4): off, on, on, on
2 查看EVM的MAC地址:通过wireshark抓包获取EVM板的MAC 地址是90-d7-eb-83-15-18
3 查看PC的MAC地址:通过ipconfig/all可以查看PC的MAC地址 : D4-BE-D9-1C-5D-96这两个参数在构造以太网包的时候作为入参输入
4 查看PC ip地址, 通过ipconfig
Connection-specific DNS Suffix . : apr.dhcp.ti.com
IP Address. . . . . . . . . . . . : 169.254.70.200
Subnet Mask . . . . . . . . . . . : 255.255.254.0
Default Gateway . . . . . . . . . : 157.87.42.1
5 给EVM指定一个位于同一网段的IP地址,例如169.254.70.201。在PC cmd窗口用arp –s把这个IP和EVM的MAC地址映射来。例如 arp -s 169.254.70.201 90-d7-eb-83-15-18
---------------------------------------------------------------------------------------------------------------------------
现在的问题是如何做第5步:给EVM指定一个位于同一网段的IP地址?具体该如何操作?
谢谢!