This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DVRRDK的问题5



各位高手,小弟正在阅读TI为8168处理器提供的DVRRDK软件开发包。阅读过程中遇到以下这个结构体:
 typedef struct VcapVencVdecVdis_IpcBitsCtrlFileObj {
    FILE *fpWrHdr[MCFW_IPC_BITS_MAX_NUM_CHANNELS];
    FILE *fpWrData[MCFW_IPC_BITS_MAX_NUM_CHANNELS];
    FILE *fpWrMvData[MCFW_IPC_BITS_MAX_NUM_CHANNELS];
    char    fileDirPath[MCFW_IPC_BITS_MAX_PATH_LENGTH];
    Bool    wrapOccuredHdr[MCFW_IPC_BITS_MAX_NUM_CHANNELS];
    Bool    wrapOccuredBuf[MCFW_IPC_BITS_MAX_NUM_CHANNELS];
    UInt32  maxFileSize;
    Bool    enableFWrite;
    UInt32  fwriteEnableBitMask;
} VcapVencVdecVdis_IpcBitsCtrlFileObj;
 请教其中wrapOccuredBuf成员的含义?以及wrapOccuredBuf成员与wrapOccuredHdr成员的区别?谢谢!