This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748没有外围的FLASH和DDR,只有单独一个DSP,用那个.gel文件初始化dsp

下载器用的是创龙XDS100V2, DSP之间用CCS的 TEST CONNECTION表示成功连接(附测试说明),但在下载程序时总出现以下错误.


C674X_0: GEL: Error loading file 'H:\demo\STARTE~1\STARTE~1\Tronlong_C6748.gel': line 1: no viable alt for char: C674X_0: File Loader: Verification failed: Values at address 0xC0000000 do not match Please verify target memory and memory map.
C674X_0: GEL: File: H:\demo\StarterWare\StarterWare\Application\UART1_POLL\Debug\UART1_POLL.out: a data verification error occurred, file load failed.
自己设计的硬件情况是:去掉了DDR和NAND FLASH,单调试DSP的下载程序功能。
  • 把GEL文件中DDR配置部分去掉。
  • 谢谢您的回复,问题就出在这,非常的感谢您!这个问题困扰了我两天了,感谢!
  • 程序可以下载进去,但dsp运行起来存储的内存数据出错,gel文件加载后出现以下信息,附带gel文件。

    C674X_0: Output: Target Connected.

    C674X_0: Output: ---------------------------------------------

    C674X_0: Output: Memory Map Cleared.

    C674X_0: Output: ---------------------------------------------

    C674X_0: Output: Memory Map Setup Complete.

    C674X_0: Output: ---------------------------------------------

    C674X_0: Output: KICK Unlocked.

    C674X_0: Output: ---------------------------------------------

    C674X_0: Output: PSC Enable Complete.

    C674X_0: Output: ---------------------------------------------

    C674X_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz

    C674X_0: Output: ---------------------------------------------

    C674X_0: Loader: One or more sections of your program falls into a memory region that is not writable.  These regions will not actually be written to the target.  Check your linker configuration and/or memory map.

    程序没有运行至main()函数,出现以下情况0003.C6748.gel

    有时间麻烦看看哈,多谢!