This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368播放视频问题

dm368在播放1280x1024  25hz的文件时   文件大小在3.5G左右 出现卡死现象

打印out of memary  

请问TI的专家  知道是什么问题吗?

  • 你好,

    请问除了out of memory的错误外,是否还有报其他的错误信息? 能否提供完整的log?
  • 如下是打印的log:

    (gstplayavi:580): GLib-GObject-WARNING **: IA__g_object_set_valist: passed '0' as denominator for `GstFraction'

    TIViddec2 framerate = 10 padAllocOutbufs=true numOutputBufs=300

    Pipeline state changed from NULL to READY:

    [   61.370000] avidemux:sink invoked oom-killer: gfp_mask=0x200da, order=0, oom_adj=0

    [   61.380000] Backtrace:

    [   61.380000] [<c00285f4>] (dump_backtrace+0x0/0x114) from [<c025228c>] (dump_stack+0x18/0x1c)

    [   61.390000]  r7:00000000 r6:c209b2c0 r5:000200da r4:c19a8000

    [   61.390000] [<c0252274>] (dump_stack+0x0/0x1c) from [<c006f218>] (oom_kill_process+0x80/0x20c)

    [   61.400000] [<c006f198>] (oom_kill_process+0x0/0x20c) from [<c006f9a8>] (__out_of_memory+0x17c/0x1a0)

    [   61.410000]  r8:00000000 r7:c19a8000 r6:000004c2 r5:c209b2c0 r4:c0343558

    [   61.420000] [<c006f82c>] (__out_of_memory+0x0/0x1a0) from [<c006fa48>] (out_of_memory+0x7c/0xd8)

    [   61.430000] [<c006f9cc>] (out_of_memory+0x0/0xd8) from [<c0072a38>] (__alloc_pages_nodemask+0x40c/0x500)

    [   61.440000]  r6:000200da r5:00000000 r4:00000000

    [   61.440000] [<c007262c>] (__alloc_pages_nodemask+0x0/0x500) from [<c0080eec>] (handle_mm_fault+0x1a0/0xc84)

    [   61.450000] [<c0080d4c>] (handle_mm_fault+0x0/0xc84) from [<c002a82c>] (do_page_fault+0xf4/0x1e8)

    [   61.460000] [<c002a738>] (do_page_fault+0x0/0x1e8) from [<c0024310>] (do_DataAbort+0x3c/0x9c)

    [   61.470000] [<c00242d4>] (do_DataAbort+0x0/0x9c) from [<c0024ec4>] (ret_from_exception+0x0/0x10)

    [   61.480000] Exception stack(0xc19a9fb0 to 0xc19a9ff8)

    [   61.480000] 9fa0:                                     00039150 42609008 00000008 430e2ff0

    [   61.490000] 9fc0: 45084d12 00000000 00073bff 40e8a21c 422dd148 00000000 00000140 000a2ce0

    [   61.500000] 9fe0: 090afec0 41987990 00039148 40e6d898 20000010 ffffffff

    [   61.510000]  r8:422dd148 r7:40e8a21c r6:00073bff r5:00000000 r4:ffffffff

    [   61.510000] Mem-info:

    [   61.510000] DMA per-cpu:

    [   61.520000] CPU    0: hi:   18, btch:   3 usd:   2

    [   61.520000] active_anon:5379 inactive_anon:5282 isolated_anon:0

    [   61.520000]  active_file:10 inactive_file:33 isolated_file:0

    [   61.520000]  unevictable:0 dirty:0 writeback:0 unstable:0

    [   61.520000]  free:254 slab_reclaimable:89 slab_unreclaimable:262

    [   61.520000]  mapped:38 shmem:10 pagetables:81 bounce:0

    [   61.550000] DMA free:1016kB min:1016kB low:1268kB high:1524kB active_anon:21516kB inactive_anon:21128kB active_file:40kB inactive_file:132kB unevictable:0kB isolated(anon):0kB isolated(file):0kB present:65024kB mlocked:0kB dirty:0kB writeback:0kB mapped:152kB shmem:40kB slab_reclaimable:356kB slab_unreclaimable:1048kB kernel_stack:288kB pagetables:324kB unstable:0kB bounce:0kB writeback_tmp:0kB pages_scanned:39 all_unreclaimable? no

    [   61.590000] lowmem_reserve[]: 0 0 0

    [   61.590000] DMA: 0*4kB 1*8kB 1*16kB 1*32kB 1*64kB 1*128kB 1*256kB 1*512kB 0*1024kB 0*2048kB 0*4096kB 0*8192kB 0*16384kB = 1016kB

    [   61.600000] 53 total pagecache pages

    [   61.610000] 16384 pages of RAM

    [   61.610000] 322 free pages

    [   61.620000] 4607 reserved pages

    [   61.620000] 275 slab pages

    [   61.620000] 50 pages shared

    [   61.630000] 0 pages swap cached

    [   61.630000] Out of memory: kill process 577 (sh) score 1218 or a child

    [   61.640000] Killed process 580 (gstplayavi)

    谢谢

  • 你好,

    numOutputBufs=300这个值为什么这么大?
  • 你好

    这个值之前是默认值 录像放不出

    测试时不知这个值是否会有影响 所以对这个值进行了修改 300这个值也没有根据 请问 这会有什么影响? 这个值得具体含义我们还是没有看懂

    谢谢
  • 您好 请问 dm368的cmem内存的使用情况怎么查看啊
  • 你好,

    我建议你也看看gstreamer对memory的使用和要求,看问题是否和gstreamer有关。