This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tda2x USB1(USB3.0)不工作,插入USB3.0的设备不供电,设备无法识别



大家好,

       关于USB3.0的问题咨询下。

       我们购买了Tda2x的demo板,现在想使用USB3.0的接口,但是发现该接口不工作, 插入USB设备,设备不供电,设备不识别。

使用的sdk版本:PROCESSOR_SDK_VISION_03_01_00_00

       该文档《TDA2x ADAS Applications Processor
23mm Package (ABC Package)
Silicon Revision 2.0
》上指出该板子支持USB3.0,所以这里想咨询下,我们购买的demo板的USB3.0为什么不能用?sdk需要升级?

还是有什么其它问题需要解决?

谢谢!