This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678调试问题:error #10234-D: unresolved symbols remain



您好: 我用的板子是TMDXEVM6678L,新建一个工程,拷贝了helloworld例程中

的".c"和".cfg"文件,"Build Project"出错,输出如下:

**** Build of configuration Debug for project InternetPingPong ****

C:\ti\ccsv5\utils\bin\gmake -k all 'Building target: InternetPingPong.out' 'Invoking: C6000 Linker' "C:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --

display_error_number --diag_warning=225 --abi=eabi -z -

m"InternetPingPong.map" --warn_sections -

i"C:/ti/ccsv5/tools/compiler/c6000/lib" -

i"C:/ti/ccsv5/tools/compiler/c6000/include" --reread_libs --rom_model -o

"InternetPingPong.out" -l"./configPkg/linker.cmd"  "./resourcemgr.obj"

"./platform_osal.obj" "./NetThread.obj" "./MainThread.obj" -l"libc.a" <Linking> warning #10247-D: creating output section ".myDDRsect" without a

SECTIONS    specification

 undefined        first referenced                                                         symbol              in file                                                             ---------        ----------------                                                        Osal_paMtCsEnter C:\ti\pdk_C6678_1_0_0_20\packages\ti\drv\pa\lib

\ti.drv.pa.ae66<pa.oe66>  Osal_paMtCsExit  C:\ti\pdk_C6678_1_0_0_20\packages\ti\drv\pa\lib

\ti.drv.pa.ae66<pa.oe66>

error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "InternetPingPong.out" not    built

尝试改正方法: Include Options—>"${TI_PDK_C6678_INSTALL_DIR}/packages/ti/drv/pa" File Search Path—>"${TI_PDK_C6678_INSTALL_DIR}/packages/ti/drv/pa/lib

\ti.drv.pa.ae66" 但是错误还在,是加入文件路径的方法不对吗? 先谢过各位了!