This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AM335x利用网口启动的问题



社区的各位大神们好,请教大家关于网口启动的问题,我是使用AM3352BZCZD60这款芯片,板子是使用公司自己开发的,我已经根据官方的文档配置好SDK6.0.0.7,也可以正常编译自带的u-boot及内核,环境也配置好TFTP服务、NFS服务、DHCP服务,启动拨码也已经设置为EMAC1(SYSBOOT[0:4]   01000b),但是插上网线后上电却没反应,我的操作步骤为:

1、DHCP服务配置后,验证,DHCP可以正确分配地址;

2、编译u-boot及内核;

3、启动setup.sh脚本(这个好像是需要串口连接的,有可能出错在这一步);

4、然后手动将各种启动文件拉入TFTP服务的共享文件夹中;

5、连接网线,上电(eth0、eth1都试过)

由于网上关于AM335x网口启动的资料不多,所以大部分看TI官网的资料,全英看起来很痛苦,而且官方的资料不是专门讲一种芯片,他是同时将多种方法以及各种芯片,所以看得头皮发麻,加上本人是个小白(实习生),所以很多操作都是乱蒙的,请各位大神给小子指条明路,谢谢大家了!!!

如果可以的话,麻烦帮我讲一下整个操作流程,跪谢了!