U-Boot SPL 2018.01-00569-g7b4e473842-dirty (Aug 23 2019 - 16:38:16)
Trying to boot from eth device
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Into Ti CPSW initialization !!!
mac_addr = 0 0 0 0 e8 feInto Ti CPSW use bbb mii !!!
cpsw
cpsw Waiting for PHY auto negotiation to complete... done
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.1.113 (63 ms)
*** Warning: no boot file name; using '00000000.img'
Using cpsw device
TFTP from server 0.0.0.0; our IP address is 192.168.1.113; sending through gateway 192.168.1.1
Filename '00000000.img'.
Load address: 0x82000000
Loading: *