This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【AM335X-Y】完成对应用程序的测试,串口,can,485,LCD屏的更换



各位老师,你们好,本人新手,缺乏linux实践经验,近期从公司接收了一套AM335x的开发板,目前想测试6个串口是否可以通信,然后将6个串口改为4个can通信和2个485,然后换一个大一点的屏。
遇到的问题:

 1. 我用DB9调试口,PC端可以接收到数据,但是PC端不能发送,就是只能接收,不能不能发送和接收

 2. 我板子烧写的是米尔科技的出厂内核,测试485和can总线时候,显示找不到485接和can接口,

 3.看门狗测试程序,已经通过ls 查询到默认有  /dev/watchdog  设备,但是具体的不会操作

已经尝试过百度,csdn等网上一些资料  ,没有比较全面的,因为第一次跑linux,所以想请问有没有推荐的资料,虽然很多不懂,但从未放弃,谢谢各位TI老师