This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x Linux SDK V5.2x U-Boot TFTP load内核时,serverip没有被正确使用



你好,

我希望能从TFTP加载内核和设备树文件,NFS挂载为根文件系统,启动整个系统;

今天下午还能正常执行,但是几次重启之后,发现TFTP加载内核时,程序使用的serverip不是环境变量中设置的ip,导致zImage加载失败,如下:

Hit any key to stop autoboot:  0
Booting from network ...
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.3.199 (5 ms)
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.3.1; our IP address is 192.168.3.199
Filename 'zImage'.
Load address: 0x82000000
Loading: T T T T

手动TFTP加载内核,正常执行,如下:

=> pri serverip
serverip=192.168.3.105
=> pri ipaddr
ipaddr=192.168.3.232
=> ping 192.168.3.105
link up on port 0, speed 100, full duplex
Using cpsw device
host 192.168.3.105 is alive

=> tftp 0x82000000 zImage
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.3.105; our IP address is 192.168.3.232
Filename 'zImage'.
Load address: 0x82000000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #####
         3.3 MiB/s
done
Bytes transferred = 3887616 (3b5200 hex)

我在论坛上找到了相似的帖子,但是帮助不大:

https://e2echina.ti.com/question_answer/dsp_arm/sitara_arm/f/25/t/176292?tisearch=e2e-sitesearch&keymatch=tftp

这是什么原因呢?

在失败的信息中,我注意到了"DHCP client bound to address 192.168.3.199 (5 ms)", U-Boot中可以使用什么方法,关闭DHCP呢?