This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467初始化不了,请求指点



DM6467T,仿真器正常,CCS3.3;DM6467T能连上CCS,但是加载了GEL后,往EE2PROM里加载.OUT文件时就会出现如下的错误,请各位高手指点这是怎么回事呢?测量了板子上的电压显示都正常,电流在目前什么都没有进行的情况下是0.5A左右。

Warning:
0x60130004/-2010 @ marker 10632
Error during: Register, RTDX, Internal,
An internal error occurred in which an unsupported operation (0x00002988) was requested.

这个问题不会代表CPU有问题吧??