如题,搭载AM4376BZDNA100的核心板在使用的过程中发生内部电源短路,给此ARM供电的芯片为TPS65218。该批核心板共计30块,出现短路现象的有3块。其中一块短路引脚为xdma_event_intr1、VDDS_OSC、VDDS_CLKOUT、VDDSHV5、VDDS、VDDSHV3、USB0_CE、VDD_CORE;第二块短路引脚为VDDS_DDR(EMC实验使用强磁场干扰时芯片损坏);第三块为1.1V和3.3V短路(核心板上测量对地直流阻抗为0.8Ω左右,暂未拆下测量)。请问各位工程师朋友有没有遇到过类似的问题?大家是如何预防和解决的?