Waiting for SFT on the DM36x...
Target: Starting UART Boot...
Target: BOOTUBL
BOOTUBL commmand received. Returning CMD and command...
CMD value sent. Waiting for DONE...
Target: DONE
DONE received. Command was accepted.
Sending the UBL image
Waiting for SENDIMG sequence...
SENDIMG received. Returning ACK and header for image data...
ACK command sent. Waiting for BEGIN command...
BEGIN commmand received.
0% [ ------------------------------------------------------------ ]
Status Undefined
100%
Waiting for DONE... Image data sent.
DONE received. All bytes of image data received...
Target: Writing UBL to NAND flash
Target: Unprotecting blocks 0x00000001 through 0x00000018.
Target: NAND is write protected!
Target: Writing failed!Starting UART Boot...
Target: BOOTUBL
Waiting for SFT on the DM36x...
用的是leopardboardDM365v1.5
启动方式UART
用nanderase已经成功了
用nandflash的时候有什么需要注意的,或者说,需要在flash utils工具里面做些修改