This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于wl1837 5G热点和速率的问题



问题1:我们使用了WL1837的wifi模块,在进行性能测试的时候,发现其不能启动5G热点,信息如下:

root@NSC200:~# ./hostapd hostapd.conf
Configuration file: hostapd.conf
[ 2115.561118] wlcore: down
rfkill: Cannot open RFKILL control device
Channel 48 (primary) not allowed for AP mode, flags: 0x73 NO-IR
wlan0: IEEE 802.11 Configured channel (48) not found from the channel list of cu
rrent mode (2) IEEE 802.11a
wlan0: IEEE 802.11 Hardware does not support configured channel
Could not select hw_mode and channel. (-3)
wlan0: interface state UNINITIALIZED->DISABLED
wlan0: AP-DISABLED
wlan0: Unable to setup interface.
wlan0: interface state DISABLED->DISABLED
wlan0: AP-DISABLED
wlan0: CTRL-EVENT-TERMINATING
hostapd_free_hapd_data: Interface wlan0 wasn't started
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
[ 2115.641454] wlcore: down
root@NSC200:~#

hostapd.conf 主要配置如下:

interface=wlan0
ssid=SC200-test
driver=nl80211
channel=48
ieee80211n=1
ieee80211ac=1

hw_mode=a

require_ht=1
ht_capab=[HT40-][HT40+][SHORT-GI-20][SHORT-GI-40]

问题2:在am335x平台,使用了WL1837的wifi模块,做2.4G热点的情况下,电脑用intel ax200 wifi连接,速率显示150M,实际下载速率不超过2.1MB/s;使用博通wifi 做5G热点的情况,连接速率433下,下载速率也不超过2.1MB/s,请问是SDIO接口速率限制了码?