如问题:打算在lan8720 中去掉其晶振 采用 am335 输出时钟供给lan8720。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如问题:打算在lan8720 中去掉其晶振 采用 am335 输出时钟供给lan8720。
你好,感谢您的回复 您所说的参考AM335x 手册Rev. k第6.2.4节中的说明。我并没有找到该小结 。我找到了下面这段描述,我所理解的是 Am335 的REF_CLK和phy在同步即可。依据下面的这段描述将其配置成output 并将时钟提供给phy 也是统一了两者的时钟。你的意思是am335 的 ref_clk只能是输入么???那下面的这端Figure 14-2 是什么意思
14.2.4 Ethernet Switch RMII Clocking Details
The RMII interface reference clock pin can operate as either an input or output. When used as an input,
the clock is driven by the I/O pad. When used as an output, the pad and the RMII clock input are driven by
the internal 50-MHz reference clock from the PRCM. The operation is controlled by the
GMII_SEL[RMIIx_IO_CLK_EN] fields in the Control Module, as shown in Figure 14-2.