TI工程师您好,使用的芯片是6678,在sysbios条件下,运行网口程序时,BIOS_Start()函数运行之后进入到网络设置任务中,当运行到NC_NetStart()函数时,
do
{
rc = NC_NetStart( hCfg, NetworkOpen, NetworkClose, NetworkIPAddr );
} while( rc > 0 );
程序跑飞,报错如下:
[C66xx_0] The C6678 CPU frequency is 1000 MHz
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
Executing the SRIO DIO example on the DEVICE
Debug(Core 0): SRIO Driver has been initialized
TCP/IP Stack 'Hello World!' Application
ti.sysbios.heaps.HeapMem: line 370: assertion failure: A_invalidFree: Invalid free
xdc.runtime.Error.raise: terminating execution
请问这是什么原因呢?