This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am5728 sdk6.0对pru单emac支持问题

Other Parts Discussed in Thread: TPIC2810

根据之前的询问了解sdk6.0的版本的pru驱动已经可以支持单emac驱动

我在移植完成新的sdk之后,按照doc/devicetree/binding/net/ti-prueth.txt更改了设备树,但是pru驱动会报访问空指针的错误

使用的设备树是am572x-idk.dtb,pru部分修改如下

pruss2_eth: pruss2_eth {
		compatible = "ti,am57-prueth";
		prus = <&pru2_0>, <&pru2_1>;
		//firmware-name = "ti-pruss/am57xx-pru0-prueth-fw.elf",
		firmware-name = "",
				"ti-pruss/am57xx-pru1-prueth-fw.elf";
		sram = <&ocmcram1>;
		interrupt-parent = <&pruss2_intc>;
		mii-rt = <&pruss2_mii_rt>;
		interrupts = <20>, <21>;
		interrupt-names = "rx_red_hp", "rx_red_lp";

		/*pruss2_emac0: ethernet-mii0 {
			phy-handle = <&pruss2_eth0_phy>;
			phy-mode = "mii";
			interrupts = <20>, <22>, <23>, <26>;
			interrupt-names = "rx", "tx", "hsrprp_ptp_tx",
					  "emac_ptp_tx";
			//Filled in by bootloader 
			local-mac-address = [00 00 00 00 00 00];
		};*/

		pruss2_emac1: ethernet-mii1 {
			phy-handle = <&pruss2_eth1_phy>;
			phy-mode = "mii";
			interrupts = <21>, <23>, <24>, <27>;
			interrupt-names = "rx", "tx", "hsrprp_ptp_tx",
					  "emac_ptp_tx";
			/* Filled in by bootloader */
			local-mac-address = [00 00 00 00 00 00];
		};
	};
  • 报错的打印信息如下

    [    3.581261] mmcblk1rpmb: mmc1:0001 Q2J55L partition 3 4.00 MiB, chardev (244:0)
    [    3.590015]  mmcblk1: p1 p2 p3
    [    3.607774] dmm 4e000000.dmm: workaround for errata i878 in use
    [    3.616061] dmm 4e000000.dmm: initialized all PAT entries
    [    3.623249] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.13
    [    3.630881] omapdss_hdmi5 58040000.encoder: Dropping the link to regulator.13
    [    3.640066] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.13
    [    3.647998] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
    [    3.656299] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
    [    3.665756] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    3.672404] [drm] No driver support for vblank timestamp query.
    [    3.678383] [drm] Cannot find any crtc or sizes
    [    3.684597] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
    [    3.694439] ALSA device list:
    [    3.697423]   No soundcards found.
    [    4.339411] EXT4-fs (mmcblk0p2): recovery complete
    [    4.345276] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    4.353473] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    4.371044] devtmpfs: mounted
    [    4.376974] Freeing unused kernel memory: 2048K
    [    4.381661] Run /sbin/init as init process
    [    4.697895] systemd[1]: System time before build time, advancing clock.
    [    4.719730] [drm] Cannot find any crtc or sizes
    [    4.741507] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    4.763548] systemd[1]: Detected architecture arm.
    Welcome to Arago 2019.05!
    [    4.802438] systemd[1]: Set hostname to <am57xx-evm>.
    [    5.068796] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    [    5.085929] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    [    5.373913] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.380614] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    5.451655] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.458713] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    5.499863] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.507190] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    5.545441] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    5.580444] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Journal Socket.
             Starting Load Kernel Modules...
    [    5.688719] cmemk: loading out-of-tree module taints kernel.
    [    5.696012] CMEMK module: reference Linux version 4.19.38
    [    5.702233] allocated heap buffer 0x40500000 of size 0x100000
    [    5.708060] cmemk initialized
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [    5.729938] cryptodev: driver 1.9 loaded.
    [    5.731423] random: crng init done
    [    5.731430] random: 5 urandom warning(s) missed due to ratelimiting
    [  OK  ] Reached target Swap.
    [    5.777745] usbcore: registered new interface driver usbfs
    [    5.783338] usbcore: registered new interface driver hub
    [    5.788811] usbcore: registered new device driver usb
             Mounting POSIX Message Queue File System...
    [    5.814087] usbcore: registered new interface driver ftdi_sio
    [    5.820004] usbserial: USB Serial support registered for FTDI USB Serial Device
    [  OK  ] Listening on udev Kernel Socket.
             Starting udev Coldplug all Devices...
    [  OK  ] Listening on Process Core Dump Socket.
             Starting Create list of required st…ce nodes for the current kernel...
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    6.089357] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [  OK  ] Created slice system-serial\x2dgetty.slice.
             Starting Journal Service...
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Reached target Paths.
             Mounting Kernel Debug File System...
    [  OK  ] Created slice User and Session Slice.
    [  OK  ] Reached target Slices.
             Mounting Temporary Directory (/tmp)...
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [  OK  ] Started Journal Service.
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Started Create list of required sta…vice nodes for the current kernel.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory (/tmp).
             Starting Create Static Device Nodes in /dev...
             Mounting Kernel Configuration File System...
             Starting Apply Kernel Variables...
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Apply Kernel Variables.
    [    6.952829] systemd-journald[139]: Received request to flush runtime journal from PID 1
             Starting udev Kernel Device Manager...
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /var/volatile...
             Mounting /media/ram...
    [  OK  ] Reached target Containers.
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Mounted /var/volatile.
    [  OK  ] Mounted /media/ram.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Service...
             Starting Network Time Synchronization...
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Started Network Service.
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
             Starting Network Name Resolution...
             Starting Wait for Network to be Configured...
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Synchronized.
    [    8.571152] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
    [    8.579361] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
    [    8.617400] omap-rproc 58820000.ipu: assigned reserved memory node ipu1-memory@9d000000
    [    8.694998] remoteproc remoteproc0: 58820000.ipu is available
    [    8.730118] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
    [    8.742630] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
    [    8.773695] omap-rproc 55020000.ipu: assigned reserved memory node ipu2-memory@95800000
    [    8.796635] remoteproc remoteproc1: 55020000.ipu is available
    [    8.807399] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
    [    8.818192] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
    [    8.826934] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memory@99000000
    [  OK  ] Started Network Name Resolution.
    [    8.852118] remoteproc remoteproc2: 40800000.dsp is available
    [  OK  ] Reached target Network.
    [    8.887184] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
    [  OK  ] Reached target Host and Network Name Lookups.
    [    8.915912] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
    [    8.924075] omap-rproc 41000000.dsp: assigned reserved memory node dsp2-memory@9f000000
    [    8.944311] remoteproc remoteproc3: 41000000.dsp is available
    [    9.198092] remoteproc remoteproc1: powering up 55020000.ipu
    [    9.231695] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3747220
    [    9.239557] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    [  OK  ] Found device /dev/ttyS2.
    [    9.429257] remoteproc remoteproc0: powering up 58820000.ipu
    [    9.434979] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 6704992
    [    9.476389] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1
    [    9.628215] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    9.634519] remoteproc remoteproc0: registered virtio0 (type 7)
    [    9.640823] remoteproc remoteproc0: remote processor 58820000.ipu is now up
    [    9.682932] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    9.686083] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x65
    [    9.727724] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x66
    [    9.729722] remoteproc remoteproc1: registered virtio1 (type 7)
    [    9.729732] remoteproc remoteproc1: remote processor 55020000.ipu is now up
    [  OK  ] Started udev Coldplug all Devices.[    9.814172] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [   10.041559] Driver for 1-wire Dallas network protocol.
    [   10.053286] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659038@58:tps659038_rtc as rtc0
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [   10.319915] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode
    [   10.346378] omap_gpio 48057000.gpio: Could not set line 16 debounce to 20000 microseconds (-22)
    [   10.355299] ov2659 0-0030: Sensor detection failed (3030, 0)
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [   10.459074] omap_rtc 48838000.rtc: registered as rtc1
    [   10.466386] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
    [   10.479914] omap-des 480a5000.des: will run requests pump with realtime priority
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
    [   10.550757] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d
             Starting rng-tools.service...
    [   10.592044] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered.
             Starting Simple Network Management Protocol (SNMP) Daemon....
             Starting TI IPC Daemon...
             Starting Print notice about GPLv3 packages...
    [   10.995211] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
    [  OK  ] Started D-Bus System Message Bus.
    [  OK  ] Started Redis In-Memory Data Store.
    [   11.113384] vpe 489d0000.vpe: Device registered as /dev/video0
    [   11.125750] remoteproc remoteproc2: powering up 40800000.dsp
    [   11.133997] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 20384784
    [   11.152977] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
    [   11.158870] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
    [   11.183057] phy phy-4a084000.phy.3: Linked as a consumer to regulator.21
    [   11.222348] remoteproc remoteproc3: powering up 41000000.dsp
    [   11.230104] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
    [   11.236091] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [   11.240138] phy phy-4a085000.phy.4: Linked as a consumer to regulator.21
    [   11.249891] remoteproc remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 20384784
    [   11.250059] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
    [   11.250099] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
    [   11.280369] CAN device driver interface
    [   11.308287] SCSI subsystem initialized
    [   11.333567] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=3f02162f, irq=89)
    [   11.375653] virtio_rpmsg_bus virtio2: rpmsg host is online
    [   11.375741] remoteproc remoteproc2: registered virtio2 (type 7)
    [   11.375750] remoteproc remoteproc2: remote processor 40800000.dsp is now up
    [   11.377843] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x3d
    [   11.456724] virtio_rpmsg_bus virtio3: rpmsg host is online
    [   11.456812] remoteproc remoteproc3: registered virtio3 (type 7)
    [   11.456821] remoteproc remoteproc3: remote processor 41000000.dsp is now up
    [   11.456968] virtio_rpmsg_bus virtio3: creating channel rpmsg-proto addr 0x3d
    [   11.496088] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
    [   11.501950] omap-aes 4b500000.aes: will run requests pump with realtime priority
    [   11.591759] net eth0: initializing cpsw version 1.15 (0)
    [   11.596213] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
    [   11.605768] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1
    [   11.605844] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [   11.605856] ahci 4a140000.sata: flags: 64bit ncq sntf pm led clo only pmp pio slum part ccc apst 
    [   11.617481] omap-aes 4b700000.aes: will run requests pump with realtime priority
    [   11.617825] vip 48990000.vip: loading firmware vpdma-1b8.bin
    [   11.649793] vip 48990000.vip: VPDMA firmware loaded
    [   11.660406] scsi host0: ahci
    [   11.709903] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 81
    [   11.715910] Micrel KSZ9031 Gigabit PHY 48485000.mdio:00: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
    [   11.731175] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [   11.852489] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
    [   11.990236] net eth1: initializing cpsw version 1.15 (0)
    [   11.997884] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
    [   11.997895] omap-hdmi-audio omap-hdmi-audio.0.auto: ASoC: no DMI vendor name!
    [   12.042317] ata1: SATA link down (SStatus 0 SControl 300)
    [   12.110660] Micrel KSZ9031 Gigabit PHY 48485000.mdio:01: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
    [   12.117846] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
    [   12.529703] davinci_mdio 4b2b2400.mdio: davinci mdio revision 1.6, bus freq 1000000
    [   12.529714] libphy: 4b2b2400.mdio: probed
    [   12.529981] mdio_bus 4b2b2400.mdio: MDIO device at address 0 is missing.
    [   12.620347] davinci_mdio 4b2b2400.mdio: phy[1]: device 4b2b2400.mdio:01, driver TI TLK10X 10/100 Mbps PHY
    [   12.626015] remoteproc remoteproc4: 4b234000.pru is available
    [   12.626193] pru-rproc 4b234000.pru: PRU rproc node pru@4b234000 probed successfully
    [   12.626616] remoteproc remoteproc5: 4b238000.pru is available
    [   12.626780] pru-rproc 4b238000.pru: PRU rproc node pru@4b238000 probed successfully
    [   12.627187] remoteproc remoteproc6: 4b2b4000.pru is available
    [   12.627375] pru-rproc 4b2b4000.pru: PRU rproc node pru@4b2b4000 probed successfully
    [   12.627742] remoteproc remoteproc7: 4b2b8000.pru is available
    [   12.627888] pru-rproc 4b2b8000.pru: PRU rproc node pru@4b2b8000 probed successfully
    [   12.664652] prueth pruss2_eth: port 2: using random MAC addr: 6e:0d:36:4c:19:13
    [   12.781685] prueth pruss2_eth: pruss_fw_drop_untagged_vlan 0
    [   12.781701] prueth pruss2_eth: pruss MC Mask (Port 1) ff:ff:ff:ff:ff:ff
    [   12.781744] prueth pruss2_eth: request for sync latch pins failed: -19
    [   12.783302] prueth pruss2_eth: TI PRU ethernet (type 0) driver initialized
    [  OK  ] Started Periodic Command Scheduler.
             Starting uim-sysfs.service...
             Starting RPC Bind Service...
             Starting Login Service...
             Starting Enable and configure wl18xx bluetooth stack...
    [  OK  ] Started Job spooling tools.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Permit User Sessions...
             Starting TI MultiCore Tools Daemon...
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Reached target Timers.
             Starting Lightning Fast Webserver With Light System Requirements...
    [  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
    [  OK  ] Started Reboot and dump vmcore via kexec.
    [  OK  ] Started rng-tools.service.
    [  OK  ] Started TI IPC Daemon.
    [  OK  ] Started RPC Bind Service.
    [  OK  ] Started Enable and configure wl18xx bluetooth stack.
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started TI MultiCore Tools Daemon.
    [  OK  ] Started Lightning Fast Webserver With Light System Requirements.
    [   16.247484] cpsw 48484000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx
    [   16.264069] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
    [   18.047338] rpmsg_rpc virtio1.rpmsg-rpc.-1.101: probing service dce-callback with src 1024 dst 101
    [   18.065487] NET: Registered protocol family 45
    [   18.088828] rpmsg_rpc virtio1.rpmsg-rpc.-1.101: published functions = 4
    [   18.096606] rpmsg_rpc virtio1.rpmsg-rpc.-1.102: probing service rpmsg-dce with src 1025 dst 102
    [   18.132672] rpmsg_rpc virtio1.rpmsg-rpc.-1.102: published functions = 9
    [   18.348376] dwc3 48890000.usb: Failed to get clk 'ref': -2
    [   18.396048] dwc3 488d0000.usb: Failed to get clk 'ref': -2
    [   19.730488] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [   19.741752] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
    [   19.765214] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
    [   19.776196] xhci-hcd xhci-hcd.1.auto: irq 181, io mem 0x48890000
    [   19.785439] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [   19.794308] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   19.812454] usb usb1: Product: xHCI Host Controller
    [   19.825032] usb usb1: Manufacturer: Linux 4.19.38-rt19-g1224cd679e xhci-hcd
    [   19.833486] usb usb1: SerialNumber: xhci-hcd.1.auto
    [   19.842175] pruss_intc_irq_set_affinity: event 21 not configured: ch = -1, host = -1
    [   19.842311] pruss_intc_irq_set_affinity: event 23 not configured: ch = -1, host = -1
    [   19.842399] pruss_intc_irq_set_affinity: event 27 not configured: ch = -1, host = -1
    [   19.855133] iep ptp bc clkid -1
    [   19.900904] Unable to handle kernel NULL pointer dereference at virtual address 000000f0
    [   19.909148] pgd = d1b2bca8
    [   19.911913] [000000f0] *pgd=ad125003, *pmd=00000000
    [   19.919185] Internal error: Oops: a06 [#1] PREEMPT SMP ARM
    [   19.919188] Modules linked in: xhci_plat_hcd(+) xhci_hcd dwc3 udc_core rpmsg_proto rpmsg_rpc ti_prueth pru_rproc pruss irq_pruss_intc snd_soc_omap_hdmi pvrsrvkm(O) ahci_platform ti_vip libahci_platform libahci omap_aes_driver libata c_can_platform c_can can_dev scsi_mod pruss_soc_bus omap_sham omap_wdt phy_omap_usb2 ti_vpe ti_sc ti_csc ti_vpdma dwc3_omap omap_des rtc_omap extcon_palmas ov2659 omap_hdq des_generic v4l2_fwnode wire crypto_engine gpio_pisosr gpio_tpic2810 omap_crypto rtc_palmas omap_remoteproc virtio_rpmsg_bus rpmsg_core remoteproc sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common gdbserverproxy(O) cryptodev(O) cmemk(O)
    [   19.919325] CPU: 0 PID: 166 Comm: systemd-network Tainted: G           O      4.19.38-rt19-g1224cd679e #8
    [   19.919328] Hardware name: Generic DRA74X (Flattened Device Tree)
    [   19.919342] PC is at memcpy+0x270/0x330
    [   19.919345] LR is at   (null)
    [   19.919349] pc : [<c099f590>]    lr : [<00000000>]    psr: 600b0013
    [   19.919353] sp : ed1d7a74  ip : 00000000  fp : ed1d7ae4
    [   19.919357] r10: ec6e09ee  r9 : 00000000  r8 : ec6e0aaa
    [   19.919361] r7 : bf379178  r6 : ec6e0840  r5 : ed1ed800  r4 : ec6e0840
    [   19.919365] r3 : 00000000  r2 : ffffffe4  r1 : ec6e0ab0  r0 : 000000f0
    [   19.919371] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    [   19.919376] Control: 30c5387d  Table: adbff480  DAC: fffffffd
    [   19.919382] Process systemd-network (pid: 166, stack limit = 0xc8cc9833)
    [   19.919386] Stack: (0xed1d7a74 to 0xed1d8000)
    [   19.919392] 7a60:                                              000000f0 ec6e0840 bf3720e4
    [   19.919399] 7a80: 05f10000 00000000 00000000 ed1d7af4 00000000 bf377b40 00001002 00000000
    [   19.919420] 7aa0: ed1ed800 00000000 ec6e0ab8 ec6e0978 40300000 ed1edd80 ed1d7ae4 ed1ed800
    [   19.919441] 7ac0: c1007488 00000000 bf377b40 ed1ed82c ed328010 00000000 ed1d7b24 ed1d7ae8
    [   19.919449] 7ae0: c0863ad8 bf3708c8 c1007488 00001002 ed1d7b0c ed1ed800 00000000 ce640771
    [   19.919455] 7b00: ed1d7b24 ed1ed800 00000001 00001003 c1007488 00001002 ed1d7b64 ed1d7b28
    [   19.919461] 7b20: c0863ed0 c0863a10 00000000 00000000 00000000 00000000 00000000 ce640771
    [   19.919467] 7b40: ed1ed800 00001002 00000000 ed1ed944 ed1d7cfc ed328010 ed1d7b8c ed1d7b68
    [   19.919473] 7b60: c0863f50 c0863d70 ed1ed800 c1007488 ed1d7c2c ed2fc6c0 ed1d7cfc ed328010
    [   19.919478] 7b80: ed1d7c14 ed1d7b90 c0879b70 c0863f3c eed490c0 eda5dac0 ed1d7d9c bf377b40
    [   19.919484] 7ba0: c0255934 c025588c ed1d7c0c eda5dac0 eed490c0 00000000 ed1d7c0c eda5e0bc
    [   19.919490] 7bc0: eed490c0 00000010 00000033 ed328028 ed1d7c2c 0000001a 00000000 ed328000
    [   19.919496] 7be0: ed1d7c14 ce640771 c054b804 c1007488 ed328000 ed1d7d9c ed2fc6c0 c1048240
    [   19.919501] 7c00: ed328010 ed328000 ed1d7d34 ed1d7c18 c087a3ac c0879880 ed1d7c2c ed1d7cfc
    [   19.919507] 7c20: 00000000 edbbf000 ed1d7c5c 00000000 00000000 00000000 00000000 00000000
    [   19.919512] 7c40: 00000000 00000000 00000000 00000000 00000000 ed328020 00000000 00000000
    [   19.919517] 7c60: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   19.919522] 7c80: 00000000 00000000 00000000 00000000 00000000 ed328028 00000000 00000000
    [   19.919527] 7ca0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   19.919532] 7cc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   19.919538] 7ce0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 c0236e00
    [   19.919543] 7d00: ed1d7d24 ed1d7d10 c08a0110 ce640771 c087a2b8 c1007488 c109135c ed2fc6c0
    [   19.919549] 7d20: 00000000 00000000 ed1d7d94 ed1d7d38 c08763b0 c087a2c4 ed12b180 c1091344
    [   19.919554] 7d40: c1091344 ed1d7d9c c1007488 c0c3a968 c02542d8 ed1d7d54 ed1d7d54 60000013
    [   19.919560] 7d60: 00000000 ce640771 c1007488 ed2fc6c0 c1007488 c0876274 ed328000 00000038
    [   19.919565] 7d80: c1007488 00000000 ed1d7de4 ed1d7d98 c08a3ec0 c0876280 ed305400 00000000
    [   19.919570] 7da0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 ce640771
    [   19.919576] 7dc0: eea2b800 eea2b800 ed991400 00000038 ed2fc6c0 00000000 ed1d7df4 ed1d7de8
    [   19.919581] 7de0: c0876270 c08a3e0c ed1d7e24 ed1d7df8 c08a361c c0876264 7fffffff ce640771
    [   19.919587] 7e00: 00000008 ed1d7eb4 c1007488 ed991400 ed2fc6c0 006000c0 ed1d7e84 ed1d7e28
    [   19.919592] 7e20: c08a3918 c08a3494 c09ba85c c0254408 ed1d7e54 ed1d7e40 00000000 00000038
    [   19.919598] 7e40: ee9fb800 00000000 000000a6 000003e1 000003de ce640771 c0253b98 00000000
    [   19.919604] 7e60: c1007488 ee506c00 00000000 bee1f94c ed1d6000 00000122 ed1d7e94 ed1d7e88
    [   19.919609] 7e80: c083e968 c08a376c ed1d7f8c ed1d7e98 c083fa50 c083e958 ed1d7ebc c0254408
    [   19.919615] 7ea0: ed1d7ecc 00000000 00000000 004fc590 00000038 ed1d7ee4 00000010 00000001
    [   19.919621] 7ec0: 00000000 00000000 ed1d7eb4 00000000 ed1d7f0c 00000000 00000000 00000000
    [   19.919628] 7ee0: ed1d7f0c 00000010 00000000 00000000 00000000 ece3e210 ed147910 ecc04b40
    [   19.919634] 7f00: ed1d7f1c ed1d7f10 c0299468 c0299224 ed1d7f54 ed1d7f20 c0357798 c029945c
    [   19.919639] 7f20: 00000020 00000000 ed1b4000 00000000 ed12b74c ed12b180 c1053d70 ed12b77c
    [   19.919645] 7f40: ed1b4000 00000006 ed1d7f64 ed1d7f58 c03578d4 c03576b0 ed1d7f8c ce640771
    [   19.919651] 7f60: c024a4c0 ce640771 c0201204 bee1f94c 00000010 004e65c8 00000122 c0201204
    [   19.919656] 7f80: ed1d7fa4 ed1d7f90 c083fab4 c083f990 bee1f94c 00000010 00000000 ed1d7fa8
    [   19.919662] 7fa0: c0201000 c083fa9c bee1f94c 00000010 00000003 004fc590 00000038 00000000
    [   19.919667] 7fc0: bee1f94c 00000010 004e65c8 00000122 00496215 004f7298 00000000 004fc5d0
    [   19.919673] 7fe0: 00000000 bee1f928 b6efc59d b6e04168 60000010 00000003 00000000 00000000
    [   19.919676] Backtrace: 
    [   19.919710] [<bf3708bc>] (emac_ndo_open [ti_prueth]) from [<c0863ad8>] (__dev_open+0xd4/0x158)
    [   19.919718]  r10:00000000 r9:ed328010 r8:ed1ed82c r7:bf377b40 r6:00000000 r5:c1007488
    [   19.919721]  r4:ed1ed800
    [   19.919732] [<c0863a04>] (__dev_open) from [<c0863ed0>] (__dev_change_flags+0x16c/0x1cc)
    [   19.919739]  r8:00001002 r7:c1007488 r6:00001003 r5:00000001 r4:ed1ed800
    [   19.919750] [<c0863d64>] (__dev_change_flags) from [<c0863f50>] (dev_change_flags+0x20/0x50)
    [   19.919756]  r9:ed328010 r8:ed1d7cfc r7:ed1ed944 r6:00000000 r5:00001002 r4:ed1ed800
    [   19.919766] [<c0863f30>] (dev_change_flags) from [<c0879b70>] (do_setlink+0x2fc/0xa44)
    [   19.919772]  r9:ed328010 r8:ed1d7cfc r7:ed2fc6c0 r6:ed1d7c2c r5:c1007488 r4:ed1ed800
    [   19.919778] [<c0879874>] (do_setlink) from [<c087a3ac>] (rtnl_setlink+0xf4/0x140)
    [   19.919785]  r10:ed328000 r9:ed328010 r8:c1048240 r7:ed2fc6c0 r6:ed1d7d9c r5:ed328000
    [   19.919788]  r4:c1007488
    [   19.919797] [<c087a2b8>] (rtnl_setlink) from [<c08763b0>] (rtnetlink_rcv_msg+0x13c/0x308)
    [   19.919803]  r9:00000000 r8:00000000 r7:ed2fc6c0 r6:c109135c r5:c1007488 r4:c087a2b8
    [   19.919815] [<c0876274>] (rtnetlink_rcv_msg) from [<c08a3ec0>] (netlink_rcv_skb+0xc0/0x118)
    [   19.919821]  r10:00000000 r9:c1007488 r8:00000038 r7:ed328000 r6:c0876274 r5:c1007488
    [   19.919824]  r4:ed2fc6c0
    [   19.919834] [<c08a3e00>] (netlink_rcv_skb) from [<c0876270>] (rtnetlink_rcv+0x18/0x1c)
    [   19.919839]  r8:00000000 r7:ed2fc6c0 r6:00000038 r5:ed991400 r4:eea2b800
    [   19.919848] [<c0876258>] (rtnetlink_rcv) from [<c08a361c>] (netlink_unicast+0x194/0x210)
    [   19.919858] [<c08a3488>] (netlink_unicast) from [<c08a3918>] (netlink_sendmsg+0x1b8/0x3a4)
    [   19.919864]  r9:006000c0 r8:ed2fc6c0 r7:ed991400 r6:c1007488 r5:ed1d7eb4 r4:00000008
    [   19.919874] [<c08a3760>] (netlink_sendmsg) from [<c083e968>] (sock_sendmsg+0x1c/0x2c)
    [   19.919880]  r10:00000122 r9:ed1d6000 r8:bee1f94c r7:00000000 r6:ee506c00 r5:c1007488
    [   19.919883]  r4:00000000
    [   19.919892] [<c083e94c>] (sock_sendmsg) from [<c083fa50>] (__sys_sendto+0xcc/0x10c)
    [   19.919899] [<c083f984>] (__sys_sendto) from [<c083fab4>] (sys_sendto+0x24/0x2c)
    [   19.919905]  r8:c0201204 r7:00000122 r6:004e65c8 r5:00000010 r4:bee1f94c
    [   19.919914] [<c083fa90>] (sys_sendto) from [<c0201000>] (ret_fast_syscall+0x0/0x54)
    [   19.919917] Exception stack(0xed1d7fa8 to 0xed1d7ff0)
    [   19.919924] 7fa0:                   bee1f94c 00000010 00000003 004fc590 00000038 00000000
    [   19.919930] 7fc0: bee1f94c 00000010 004e65c8 00000122 00496215 004f7298 00000000 004fc5d0
    [   19.919934] 7fe0: 00000000 bee1f928 b6efc59d b6e04168
    [   19.919941] Code: e1a0382e e491e004 e25cc004 e183380e (e4803004) 
    [   20.285928] hub 1-0:1.0: USB hub found
    [   20.286589] hub 1-0:1.0: 1 port detected
    [   20.306768] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [   20.306792] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
    [   20.306812] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0  SuperSpeed
    [   20.306944] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [   20.307167] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [   20.307178] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   20.307186] usb usb2: Product: xHCI Host Controller
    [   20.307194] usb usb2: Manufacturer: Linux 4.19.38-rt19-g1224cd679e xhci-hcd
    [   20.307202] usb usb2: SerialNumber: xhci-hcd.1.auto
    [   20.326386] hub 2-0:1.0: USB hub found
    [   20.326441] hub 2-0:1.0: 1 port detected
    [   20.342912] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [   20.343122] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 3
    [   20.343726] xhci-hcd xhci-hcd.2.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
    [   20.349765] xhci-hcd xhci-hcd.2.auto: irq 182, io mem 0x488d0000
    [   20.350662] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [   20.350673] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   20.350681] usb usb3: Product: xHCI Host Controller
    [   20.350688] usb usb3: Manufacturer: Linux 4.19.38-rt19-g1224cd679e xhci-hcd
    [   20.350696] usb usb3: SerialNumber: xhci-hcd.2.auto
    [   20.358654] hub 3-0:1.0: USB hub found
    [   20.358706] hub 3-0:1.0: 1 port detected
    [   20.359432] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [   20.359451] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 4
    [   20.359469] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0  SuperSpeed
    [   20.359593] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
    [   20.359872] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [   20.359883] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   20.359891] usb usb4: Product: xHCI Host Controller
    [   20.359899] usb usb4: Manufacturer: Linux 4.19.38-rt19-g1224cd679e xhci-hcd
    [   20.359906] usb usb4: SerialNumber: xhci-hcd.2.auto
    [   20.369921] hub 4-0:1.0: USB hub found
    [   20.369980] hub 4-0:1.0: 1 port detected
    [   20.910969] ---[ end trace 0000000000000002 ]---
    [   21.072413] ------------[ cut here ]------------
    [   21.072431] WARNING: CPU: 0 PID: 166 at kernel/locking/rtmutex.h:28 rt_mutex_slowlock_locked+0x23c/0x2d4
    [   21.072433] rtmutex deadlock detected
    [   21.072436] Modules linked in: xhci_plat_hcd xhci_hcd dwc3 udc_core rpmsg_proto rpmsg_rpc ti_prueth pru_rproc pruss irq_pruss_intc snd_soc_omap_hdmi pvrsrvkm(O) ahci_platform ti_vip libahci_platform libahci omap_aes_driver libata c_can_platform c_can can_dev scsi_mod pruss_soc_bus omap_sham omap_wdt phy_omap_usb2 ti_vpe ti_sc ti_csc ti_vpdma dwc3_omap omap_des rtc_omap extcon_palmas ov2659 omap_hdq des_generic v4l2_fwnode wire crypto_engine gpio_pisosr gpio_tpic2810 omap_crypto rtc_palmas omap_remoteproc virtio_rpmsg_bus rpmsg_core remoteproc sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common gdbserverproxy(O) cryptodev(O) cmemk(O)
    [   21.072563] CPU: 0 PID: 166 Comm: systemd-network Tainted: G      D    O      4.19.38-rt19-g1224cd679e #8
    [   21.072566] Hardware name: Generic DRA74X (Flattened Device Tree)
    [   21.072569] Backtrace: 
    [   21.072582] [<c020c6a8>] (dump_backtrace) from [<c020c9e0>] (show_stack+0x18/0x1c)
    [   21.072589]  r7:c0bbde24 r6:60070193 r5:00000000 r4:c1050664
    [   21.072598] [<c020c9c8>] (show_stack) from [<c09a1084>] (dump_stack+0x90/0xa4)
    [   21.072610] [<c09a0ff4>] (dump_stack) from [<c022cf60>] (__warn+0xdc/0xf8)
    [   21.072615]  r7:c0bbde24 r6:00000009 r5:00000000 r4:ed1d766c
    [   21.072625] [<c022ce84>] (__warn) from [<c022cb7c>] (warn_slowpath_fmt+0x50/0x6c)
    [   21.072630]  r9:00000002 r8:ed1d76f8 r7:00000000 r6:c1091344 r5:c0bbde08 r4:c1007488
    [   21.072639] [<c022cb30>] (warn_slowpath_fmt) from [<c09b83d0>] (rt_mutex_slowlock_locked+0x23c/0x2d4)
    [   21.072642]  r3:ffffffdd r2:c0bbde08
    [   21.072645]  r5:c1007488 r4:0000e000
    [   21.072652] [<c09b8194>] (rt_mutex_slowlock_locked) from [<c09b84d8>] (rt_mutex_slowlock.constprop.13+0x70/0xb4)
    [   21.072657]  r10:00000000 r9:60070113 r8:ed1d76f8 r7:c1091344 r6:00000000 r5:00000000
    [   21.072660]  r4:c1007488
    [   21.072666] [<c09b8468>] (rt_mutex_slowlock.constprop.13) from [<c09b893c>] (__rt_mutex_lock_state+0x94/0xbc)
    [   21.072671]  r10:ed1c3d08 r9:00000008 r8:ecc04500 r7:ee805b10 r6:00000000 r5:00000002
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPLv3 packages[   21.072674]  r4:c1091344
    [   21.072681] [<c09b88a8>] (__rt_mutex_lock_state) from [<c09ba91c>] (_mutex_lock+0x14/0x18)
    [   21.072684]  r5:ecc31600 r4:ede8d800
    [   21.072694] [<c09ba908>] (_mutex_lock) from [<c0873698>] (rtnl_lock+0x18/0x1c)
    [   21.072703] [<c0873680>] (rtnl_lock) from [<c094f758>] (ipv6_sock_mc_close+0x34/0x44)
    [   21.072712] [<c094f724>] (ipv6_sock_mc_close) from [<c091ce30>] (inet6_release+0x24/0x40)
    [   21.072716]  r5:ecc31600 r4:ede8d800
    [   21.072725] [<c091ce0c>] (inet6_release) from [<c083d2bc>] (__sock_release+0x48/0xc0)
    [   21.072728]  r5:ecc316b8 r4:ecc31600
    [   21.072734] [<c083d274>] (__sock_release) from [<c083d34c>] (sock_close+0x18/0x20)
    [   21.072738]  r7:ee805b10 r6:ecc31620 r5:00000000 r4:ed1c3d00
    [   21.072746] [<c083d334>] (sock_close) from [<c0357734>] (__fput+0x90/0x1d0)
    [   21.072751] [<c03576a4>] (__fput) from [<c03578d4>] (____fput+0x10/0x14)
    [   21.072756]  r10:ed12b180 r9:ed1c3d00 r8:ed12b77c r7:c1053d70 r6:ed12b180 r5:ed12b74c
    [   21.072759]  r4:ed1c3c00
    [   21.072766] [<c03578c4>] (____fput) from [<c024a4d8>] (task_work_run+0x9c/0xb8)
    [   21.072773] [<c024a43c>] (task_work_run) from [<c0230a2c>] (do_exit+0x3a4/0xb18)
    [   21.072778]  r9:00000000 r8:ed1d786c r7:ed1d6000 r6:ed999d90 r5:ed999d40 r4:ed12b180
    [   21.072784] [<c0230688>] (do_exit) from [<c020bd78>] (die+0x34c/0x358)
    [   21.072786]  r7:ed1d6000
    [   21.072795] [<c020ba2c>] (die) from [<c0213ec4>] (__do_kernel_fault.part.0+0x6c/0x7c)
    [   21.072801]  r10:ed999d90 r9:c107b350 r8:000000f0 r7:ed999d40 r6:00000a06 r5:ed1d7a20
    [   21.072803]  r4:000000f0
    [   21.072812] [<c0213e58>] (__do_kernel_fault.part.0) from [<c0214258>] (do_bad_area+0x0/0x84)
    [   21.072816]  r7:00000a06 r4:ed1d7a20
    [   21.072825] [<c0213ed4>] (do_page_fault) from [<c02143c8>] (do_translation_fault+0xec/0x118)
    [   21.072831]  r10:ec6e09ee r9:ed1d6000 r8:00000a06 r7:c100c084 r6:000000f0 r5:00000a06
    [   21.072833]  r4:c1007488
    [   21.072842] [<c02142dc>] (do_translation_fault) from [<c021443c>] (do_DataAbort+0x48/0xe0)
    [   21.072848]  r9:ed1d6000 r8:ed1d7a20 r7:c100c084 r6:000000f0 r5:00000a06 r4:c1007488
    [   21.072856] [<c02143f4>] (do_DataAbort) from [<c0201970>] (__dabt_svc+0x50/0x80)
    [   21.072860] Exception stack(0xed1d7a20 to 0xed1d7a68)
    [   21.072866] 7a20: 000000f0 ec6e0ab0 ffffffe4 00000000 ec6e0840 ed1ed800 ec6e0840 bf379178
    [   21.072871] 7a40: ec6e0aaa 00000000 ec6e09ee ed1d7ae4 00000000 ed1d7a74 00000000 c099f590
    [   21.072874] 7a60: 600b0013 ffffffff
    [   21.072880]  r9:ed1d6000 r8:ec6e0aaa r7:ed1d7a54 r6:ffffffff r5:600b0013 r4:c099f590
    [   21.072908] [<bf3708bc>] (emac_ndo_open [ti_prueth]) from [<c0863ad8>] (__dev_open+0xd4/0x158)
    [   21.072915]  r10:00000000 r9:ed328010 r8:ed1ed82c r7:bf377b40 r6:00000000 r5:c1007488
    [   21.072917]  r4:ed1ed800
    [   21.072927] [<c0863a04>] (__dev_open) from [<c0863ed0>] (__dev_change_flags+0x16c/0x1cc)
    [   21.072932]  r8:00001002 r7:c1007488 r6:00001003 r5:00000001 r4:ed1ed800
    [   21.072941] [<c0863d64>] (__dev_change_flags) from [<c0863f50>] (dev_change_flags+0x20/0x50)
    [   21.072947]  r9:ed328010 r8:ed1d7cfc r7:ed1ed944 r6:00000000 r5:00001002 r4:ed1ed800
    [   21.072955] [<c0863f30>] (dev_change_flags) from [<c0879b70>] (do_setlink+0x2fc/0xa44)
    [   21.072961]  r9:ed328010 r8:ed1d7cfc r7:ed2fc6c0 r6:ed1d7c2c r5:c1007488 r4:ed1ed800
    [   21.072966] [<c0879874>] (do_setlink) from [<c087a3ac>] (rtnl_setlink+0xf4/0x140)
    [   21.072972]  r10:ed328000 r9:ed328010 r8:c1048240 r7:ed2fc6c0 r6:ed1d7d9c r5:ed328000
    [   21.072974]  r4:c1007488
    [   21.072982] [<c087a2b8>] (rtnl_setlink) from [<c08763b0>] (rtnetlink_rcv_msg+0x13c/0x308)
    [   21.072987]  r9:00000000 r8:00000000 r7:ed2fc6c0 r6:c109135c r5:c1007488 r4:c087a2b8
    [   21.072998] [<c0876274>] (rtnetlink_rcv_msg) from [<c08a3ec0>] (netlink_rcv_skb+0xc0/0x118)
    [   21.073004]  r10:00000000 r9:c1007488 r8:00000038 r7:ed328000 r6:c0876274 r5:c1007488
    [   21.073006]  r4:ed2fc6c0
    [   21.073015] [<c08a3e00>] (netlink_rcv_skb) from [<c0876270>] (rtnetlink_rcv+0x18/0x1c)
    [   21.073020]  r8:00000000 r7:ed2fc6c0 r6:00000038 r5:ed991400 r4:eea2b800
    [   21.073029] [<c0876258>] (rtnetlink_rcv) from [<c08a361c>] (netlink_unicast+0x194/0x210)
    [   21.073038] [<c08a3488>] (netlink_unicast) from [<c08a3918>] (netlink_sendmsg+0x1b8/0x3a4)
    [   21.073043]  r9:006000c0 r8:ed2fc6c0 r7:ed991400 r6:c1007488 r5:ed1d7eb4 r4:00000008
    [   21.073052] [<c08a3760>] (netlink_sendmsg) from [<c083e968>] (sock_sendmsg+0x1c/0x2c)
    [   21.073057]  r10:00000122 r9:ed1d6000 r8:bee1f94c r7:00000000 r6:ee506c00 r5:c1007488
    [   21.073059]  r4:00000000
    [   21.073067] [<c083e94c>] (sock_sendmsg) from [<c083fa50>] (__sys_sendto+0xcc/0x10c)
    [   21.073075] [<c083f984>] (__sys_sendto) from [<c083fab4>] (sys_sendto+0x24/0x2c)
    [   21.073080]  r8:c0201204 r7:00000122 r6:004e65c8 r5:00000010 r4:bee1f94c
    [   21.073087] [<c083fa90>] (sys_sendto) from [<c0201000>] (ret_fast_syscall+0x0/0x54)
    [   21.073090] Exception stack(0xed1d7fa8 to 0xed1d7ff0)
    [   21.073096] 7fa0:                   bee1f94c 00000010 00000003 004fc590 00000038 00000000
    [   21.073101] 7fc0: bee1f94c 00000010 004e65c8 00000122 00496215 004f7298 00000000 004fc5d0
    [   21.073105] 7fe0: 00000000 bee1f928 b6efc59d b6e04168
    [   21.073109] ---[ end trace 0000000000000003 ]---
  • 请问您这个问题解决了吗?看您之前的帖子解决了。
    e2echina.ti.com/.../181913
  • 没有,这个就是移植完成新的内核之后,新版的pru驱动报错
  • 请问Dual EMAC 可以运行吗?
  • 不可以,因为只连接了一个phy,只使用了pru2 mii1这个,使用的时候会报错
  • 请尝试按照下面的几点修改一下 am57xx-idk-common.dtsi

    1) comment out the alias ethernet2:

    aliases { ...
    ethernet2 = &pruss2_emac0;
    ...
    }

    2) modify pruss2_eth node in the same way that they did for am572x-idk.dts

    3) comment out the subnode pruss2_eth0_phy:

    &pruss2_mdio {...
    pruss2_eth0_phy: ethernet-phy@0 {
    reg = <0>;
    interrupt-parent = <&gpio3>;
    interrupts = <30 IRQ_TYPE_EDGE_FALLING>;
    };
    ...
    };