This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问有6678的emif接口SRAM模式的例程吗?



Keystone_SDK_Packet包里面的emif例程是nand flash和norflash的例程,还是说sram模式配置是和nor flash配置一样的?

  • sram模式配置是和nor flash一样的,都是Async memory。
  • 我目前也设计了6678+FPGA的方式,也是6678读取FPGA内部的SRAM,采用EMIF,但是说明书上写
    70000000 73FFFFFF 64M EMIF16 CS2 Data NAND Memory
    74000000 77FFFFFF 64M EMIF16 CS3 Data NAND Memory
    78000000 7BFFFFFF 64M EMIF16 CS4 Data NOR Memory
    7C000000 7FFFFFFF 64M EMIF16 CS5 Data SRAM Memory
    如果例程是对NOR FLASH配置的,那么起始地址是78000000,而SRAM起始地址是7C000000,如果直接采用Keystone_SDK_Packet包里面的emif例程,那么配置NOR FLASH的起始地址是78000000,而我们需要对SRAM操作,按照这个表格,起始地址是7C000000,所以如果采用这个例程的话,是否需要把78000000改成7C000000?还是直接就可以使用。但是在例程里根本没有找到地址78000000
  • 新问题麻烦另起新帖,方便其他客户参考。
  • 大佬 能不能给我一份6678 EMIF与FPGA通信的例程啊 我也在做,新手有点懵逼,有偿