This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK_1.93问题



在C6000单核DSP上使用NDK1_93进行网络开发。

网络连接过程中出现如下错误。

Using MAC Address: 08-00-28-68-f2-00
Network Added: If-1:192.168.42.150
00001.018 mmBulkFree: Corrupted mem or bad ptr (800064d8)
00001.018 mmFree: Double Free
Network Removed: If-1:192.168.42.150
00001.100 mmFree: Double Free
Network is shut off

19:48 ( 29%) 13:96 ( 40%) 1:128 ( 4%) 9:256 ( 75%)
1:512 ( 16%) 0:1536 0:3072
(15360/49152 mmAlloc: 51/0/47, mmBulk: 6/0/7)

1 blocks alloced in 48 byte page
(000B)
5 blocks alloced in 256 byte page
(000A) (000A) (0000) (000A) (82DEAA44)

希望知道是什么原因引起的。

HEAP有16MB大。