This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8127 IPNC



您好:

我们买了APPRO公司的DM8127的网络摄像机。

在连上串口之后,相机中的程序跑不起来。以下是日志信息,根据日志分析是M3_VPSS没有跑起来,貌似syslink有点问题,这这边分析不出原因。麻烦帮忙分析一下。这个是买来的时候相机flash里的程序,我一点都没改过。

UBIFS: reserved for root:  3688395 bytes (3601 KiB)
./init.sh: line 5: -f: not found
numid=1,iface=MIXER,name='PCM Playback Volume'
  ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
  : values=127,127
  | dBscale-min=-63.50dB,step=0.50dB,mute=0
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
SysLink version : 2.20.02.20
SysLink module created on Date:Dec 21 2012 Time:20:22:18
Trace enabled
Trace SetFailureReason enabled
/dev/mem opened.
             Phy Addr : 0x48181560 Data : 0x00000002
secss put in low power state
             Phy AUnhandled fault: external abort on non-linefetch (0x1018) at 0x4030f000
ddr : 0x48180f10 Data : 0x00000000
             Phy Addr : 0x48180508 Data : 0x00000302
             Phy Addr : 0x48180520 Data : 0x00000002
             Phy Addr : 0x48180524 Data : 0x00000002
             Phy Addr : 0x48180528 Data : 0x00000002
             Phy Addr : 0x4c0000e4 Data : 0x00170208
             Phy Addr : 0x4d0000e4 Data : 0x00170208
             Phy Addr : 0x4c0000e4 Data : 0x00170208
             Phy Addr : 0x4d0000e4 Data : 0x00170208
DDR IOs RX is shutdown
             Phy Addr : 0x48180a04 Data : 0x00000000
        PRCM for TPPSS Initialization in Progress
             Phy Addr : 0x4818050c Data : 0x00007302
             Phy Addr : 0x48180554 Data : 0x00070002
        PRCM for TPPSS Initialization is Done
Bus error

 [host]  Setting DMM priority for [HDVICP0 ] to [1] ( 0x4e000634 = 0x00000009 )

 [host]  Setting L3 bandwidth regulator for [HDVICP0 ] to [press=[0,0] BW=900, WM Cycles=2500]
Creat queue id:0
queue id:0

 [host]  Setting DMM priority for [ISS     ] to [0] ( 0x4e000634 = 0x00800000 )
FileMngThread created
Creat queue id:32769
queue id:32769
queue id:32769
AlramThread created
Share memory init success
Creat queue id:65538
queue id:65538
Creat queue id:98307
queue id:98307
IPNC_3.50.00 (a0875405@bangvideoapps01) (gcc version 4.5.3 20110311 (pr

 [host] Attached to slave procId 1.
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

 [host] Attached to slave procId 2.

 [host] Loaded file ./firmware/ipnc_rdk_fw_m3video.xem3 on slave procId 1.
UBIFS error (pid 344): ubifs_read_node: bad node length 3149, expected 3148
UBIFS error (pid 344): ubifs_read_node: bad node at LEB 33:95104, LEB mapping status 1
UBIFS error (pid 344): do_readpage: cannot read page 101 of inode 409, error -22

 [host] Started slave procId 1.

 [host] After Ipc_loadcallback status [0x00000000]

 [host] Loaded file ./firmware/ipnc_rdk_fw_m3vpss.xem3 on slave procId 2.

 [host] Started slave procId 2.

 [host] After Ipc_loadcallback status [0x00000000]
 [m3video] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
 [m3video] 
 [m3video]  *** UTILS: CPU KHz = 400000 Khz ***
 [m3video] 
 [m3video]  110: SYSTEM  : System Common Init in progress !!!
 [m3video]  114: SYSTEM: IPC init in progress !!!
 [m3video]  117: SYSTEM: Attaching to [HOST] ...
 [m3video]  1119: SYSTEM: Attaching to [HOST] ...

 [host] After Ipc_startcallback status [0x00000000]
 [m3video]  1170: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [m3video]  1173: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  2176: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  3179: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  4182: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  5185: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  6188: SYSTEM: Attaching to [VPSS-M3] ...
 inside autorun
 sbulla: unknown partition table
 sbulla: unknown partition table
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: done

____                    _____           _         _  
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_| 
              |___|                    |___|           

Arago Project http://arago-project.org dm814x-evm ttyO0

Arago 2011.09 dm814x-evm ttyO0

dm814x-evm login: root (automatic login)
root@dm814x-evm:~#  [m3video]  7191: SYSTEM: Attaching to [VPSS-M3] ...
mkdosfs 3.0.12 (29 Oct 2011)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
There is 1 reserved sector.
Root directory contains 512 slots and uses 32 sectors.
Volume ID is 054c3d8c, no volume label.
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
Simple mixer control 'PGA',0
  Capabilities: cvolume cswitch penum
  Capture channels: Front Left - Front Right
  Limits: Capture 0 - 119
  Front Left: Capture 80 [67%] [40.00dB] [on]
  Front Right: Capture 80 [67%] [40.00dB] [on]
 [m3video]  8194: SYSTEM: Attaching to [VPSS-M3] ...
queue id:0
 [m3video]  9197: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  10200: SYSTEM: Attaching to [VPSS-M3] ...
ApproDrvInit: 3
Creat queue id:131076
queue id:131076
 [m3video]  11203: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  12206: SYSTEM: Attaching to [VPSS-M3] ...
queue id:0
 [m3video]  13209: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  14212: SYSTEM: Attaching to [VPSS-M3] ...

 [m3video]  245905: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  246908: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  247911: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  248914: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  249917: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  250920: SYSTEM: Attaching to [VPSS-M3] ...
*** Platform_startCallback: Ipc_attach timeout
        Error [0xffffffff] at Line no: 2860 in file /data/datalocal_videoapps01/user/kudva/DM812x/IPNetCam/ti_tools/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/ti81xx/Platform.c
*** Ipc_control: Platform_startCallback failed!
        Error [0xffffffff] at Line no: 853 in file /data/datalocal_videoapps01/user/kudva/DM812x/IPNetCam/ti_tools/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Ipc.c

 [host] Error in Ipc_control Ipc_CONTROLCMD_STARTCALLBACK [0xffffffff]
 [m3video]  251923: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  252926: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  253929: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  254932: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  255935: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  256938: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  257941: SYSTEM: Attaching to [VPSS-M3] ...
 [m3video]  258944: SYSTEM: Attaching to [VPSS-M3] ...