This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728内核启动时,Systemd服务花费很长的时间,且进不去cli



如下log:

U-Boot 2019.01-g463d755b90-dirty (Dec 11 2019 - 20:15:28 +0800)

CPU  : DRA752-GP ES2.0
Model: TI AM5728 BeagleBoard-X15
Board: UNKNOWN(BeagleBoard X15?) REV UNKNOWN
DRAM:  2 GiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment

Loading Environment from MMC... *** Warning - bad CRC, using default environment

Warning: fastboot.board_rev: unknown board revision
am57x_idk_lcd_detect: Failed to get I2C device 0/56 (ret 1)
Net:   
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot:  2  1  0 
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4006400 bytes read in 176 ms (21.7 MiB/s)
101295 bytes read in 6 ms (16.1 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8ffe4000, end 8ffffbae ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.79-ge669d52447 (soke@Soke) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT Thu Dec 12 18:51:21 CST 2019
[    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[    0.000000] CPU: div instructions available: patching division code
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] OF: fdt: Machine model: TI AM5728 IDK
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[    0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[    0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[    0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[    0.000000] OF: reserved mem: initialized node dsp2-memory@9f000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
[    0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier
[    0.000000] DRA752 ES2.0
[    0.000000] percpu: Embedded 15 pages/cpu @eed34000 s31372 r8192 d21876 u61440
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 472640
[    0.000000] Kernel command line: console=ttyS0,115200n8 root=PARTUUID=16b0c4ce-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 1675664K/1897472K available (8192K kernel code, 347K rwdata, 2568K rodata, 2048K init, 281K bss, 33392K reserved, 188416K cma-reserved, 1283072K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0a00000   (10208 kB)
[    0.000000]       .init : 0xc0e00000 - 0xc1000000   (2048 kB)
[    0.000000]       .data : 0xc1000000 - 0xc1056eb0   ( 348 kB)
[    0.000000]        .bss : 0xc1058000 - 0xc109e670   ( 282 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] 	Tasks RCU enabled.
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] OMAP clockevent source: timer1 at 32786 Hz
[    0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[    0.000017] Switching to timer-based delay loop, resolution 162ns
[    0.000353] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000362] OMAP clocksource: 32k_counter at 32768 Hz
[    0.000813] Console: colour dummy device 80x30
[    0.000842] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[    0.000859] pid_max: default: 32768 minimum: 301
[    0.000966] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000980] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001515] CPU: Testing write buffer coherency: ok
[    0.001553] CPU0: Spectre v2: using ICIALLU workaround
[    0.001748] /cpus/cpu@0 missing clock-frequency property
[    0.001768] /cpus/cpu@1 missing clock-frequency property
[    0.001780] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.039865] Setting up static identity map for 0x80200000 - 0x80200060
[    0.059877] Hierarchical SRCU implementation.
[    0.080063] EFI services will not be available.
[    0.099935] smp: Bringing up secondary CPUs ...
[    0.170300] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.170306] CPU1: Spectre v2: using ICIALLU workaround
[    0.170408] smp: Brought up 1 node, 2 CPUs
[    0.170419] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[    0.170427] CPU: All CPU(s) started in HYP mode.
[    0.170434] CPU: Virtualization extensions available.
[    0.170965] devtmpfs: initialized
[    0.188967] random: get_random_u32 called from bucket_table_alloc+0x108/0x234 with crng_init=0
[    0.189228] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.189418] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.189435] futex hash table entries: 512 (order: 3, 32768 bytes)
[    0.195852] pinctrl core: initialized pinctrl subsystem
[    0.196307] DMI not present or invalid.
[    0.196558] NET: Registered protocol family 16
[    0.197586] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.198506] omap_hwmod: l3_main_2 using broken dt data from ocp
[    0.402223] cpuidle: using governor ladder
[    0.402257] cpuidle: using governor menu
[    0.410504] OMAP GPIO hardware version 0.1
[    0.438445] No ATAGs?
[    0.438517] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.438531] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.438885] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[    0.438896] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[    0.439429] OMAP DMA hardware revision 0.0
[    0.449071] edma 43300000.edma: memcpy is disabled
[    0.452399] edma 43300000.edma: TI EDMA DMA engine driver
[    0.459300] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[    0.462701] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[    0.462899] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[    0.463141] omap-iommu 58882000.mmu: 58882000.mmu registered
[    0.463376] omap-iommu 55082000.mmu: 55082000.mmu registered
[    0.463735] omap-iommu 41501000.mmu: 41501000.mmu registered
[    0.463948] omap-iommu 41502000.mmu: 41502000.mmu registered
[    0.464193] iommu: Adding device 58820000.ipu to group 1
[    0.464283] iommu: Adding device 55020000.ipu to group 2
[    0.464437] iommu: Adding device 40800000.dsp to group 0
[    0.464699] iommu: Adding device 41000000.dsp to group 3
[    0.466939] palmas 0-0058: Irq flag is 0x00000004
[    0.492182] palmas 0-0058: Muxing GPIO 2b, PWM 0, LED 0
[    0.493804] SMPS12: supplied by regulator-dummy
[    0.495513] SMPS3: supplied by VMAIN
[    0.497087] SMPS45: supplied by regulator-dummy
[    0.498932] SMPS6: supplied by VMAIN
[    0.500640] SMPS7: supplied by VMAIN
[    0.502480] SMPS8: supplied by VMAIN
[    0.503759] SMPS9: supplied by VMAIN
[    0.504753] LDO1: supplied by VMAIN
[    0.511170] random: fast init done
[    0.511305] LDO2: supplied by VMAIN
[    0.521161] LDO3: supplied by VMAIN
[    0.531191] LDO4: supplied by VMAIN
[    0.541206] LDO5: supplied by regulator-dummy
[    0.541906] LDO6: supplied by regulator-dummy
[    0.542612] LDO7: supplied by regulator-dummy
[    0.543316] LDO8: supplied by regulator-dummy
[    0.544033] LDO9: supplied by VMAIN
[    0.551520] LDOLN: supplied by VMAIN
[    0.561230] LDOUSB: supplied by VMAIN
[    0.574044] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[    0.574249] media: Linux media interface: v0.10
[    0.574285] Linux video capture interface: v2.00
[    0.574368] pps_core: LinuxPPS API ver. 1 registered
[    0.574377] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.574396] PTP clock support registered
[    0.574423] EDAC MC: Ver: 3.0.0
[    0.580698] dmi: Firmware registration failed.
[    0.581088] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[    0.581372] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[    0.581707] Advanced Linux Sound Architecture Driver Initialized.
[    0.590770] clocksource: Switched to clocksource arch_sys_counter
[    0.598306] NET: Registered protocol family 2
[    0.598835] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.598899] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.599025] TCP: Hash tables configured (established 8192 bind 8192)
[    0.599093] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.599127] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.599247] NET: Registered protocol family 1
[    0.599523] RPC: Registered named UNIX socket transport module.
[    0.599534] RPC: Registered udp transport module.
[    0.599542] RPC: Registered tcp transport module.
[    0.599550] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.600426] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    0.600614] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[    0.601700] workingset: timestamp_bits=14 max_order=19 bucket_order=5
[    0.605751] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.606251] NFS: Registering the id_resolver key type
[    0.606274] Key type id_resolver registered
[    0.606282] Key type id_legacy registered
[    0.606319] ntfs: driver 2.1.32 [Flags: R/O].
[    0.607600] bounce: pool size: 64 pages
[    0.607647] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[    0.607657] io scheduler noop registered
[    0.607666] io scheduler deadline registered
[    0.607758] io scheduler cfq registered (default)
[    0.607768] io scheduler mq-deadline registered
[    0.607777] io scheduler kyber registered
[    0.612223] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[    0.614956] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
[    0.615325] OF: PCI: host bridge /ocp/axi@0/pcie@51000000 ranges:
[    0.615363] OF: PCI:    IO 0x20003000..0x20012fff -> 0x00000000
[    0.615385] OF: PCI:   MEM 0x20013000..0x2fffffff -> 0x20013000
[    1.615641] dra7-pcie 51000000.pcie: phy link never came up
[    1.615771] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[    1.615785] pci_bus 0000:00: root bus resource [bus 00-ff]
[    1.615796] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    1.615807] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[    1.616121] PCI: bus0: Fast back to back transfers disabled
[    1.616216] PCI: bus1: Fast back to back transfers enabled
[    1.616254] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[    1.616273] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    1.616588] pcieport 0000:00:00.0: Signaling PME with IRQ 173
[    1.616712] pcieport 0000:00:00.0: AER enabled with IRQ 173
[    1.619707] V3_3D: supplied by smps9
[    1.619973] vtt_fixed: supplied by V3_3D
[    1.661793] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    1.664415] console [ttyS0] disabled
[    1.664469] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 45, base_baud = 3000000) is a 8250
[    2.712613] console [ttyS0] enabled
[    2.717970] omap_rng 48090000.rng: Random Number Generator ver. 20
[    2.725090] DSS: OMAP DSS rev 6.1
[    2.730042] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[    2.738451] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[    2.758566] brd: module loaded
[    2.767088] loop: module loaded
[    2.774079] m25p80 spi0.0: unrecognized JEDEC id bytes: 00, 00, 00
[    2.780901] libphy: Fixed MDIO Bus: probed
[    2.840796] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[    2.848489] davinci_mdio 48485000.mdio: detected phy mask fffffffc
[    2.859421] libphy: 48485000.mdio: probed
[    2.863501] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver Micrel KSZ9031 Gigabit PHY
[    2.873229] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[    2.883685] cpsw 48484000.ethernet: Detected MACID = 88:3f:4a:4e:2d:4e
[    2.890295] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[    2.896721] cpsw 48484000.ethernet: ALE Table size 1024
[    2.902024] cpsw 48484000.ethernet: device node lookup for pps timer failed
[    2.909056] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[    2.916951] cpsw 48484000.ethernet: cpsw: Detected MACID = 88:3f:4a:4e:2d:4f
[    2.925191] i2c /dev entries driver
[    2.929381] IR NEC protocol handler initialized
[    2.933960] IR RC5(x/sz) protocol handler initialized
[    2.939033] IR RC6 protocol handler initialized
[    2.943620] IR JVC protocol handler initialized
[    2.948170] IR Sony protocol handler initialized
[    2.952823] IR SANYO protocol handler initialized
[    2.957548] IR Sharp protocol handler initialized
[    2.962576] IR MCE Keyboard/mouse protocol handler initialized
[    2.968435] IR XMP protocol handler initialized
[    2.978456] sdhci: Secure Digital Host Controller Interface driver
[    2.984744] sdhci: Copyright(c) Pierre Ossman
[    2.989921] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.996485] sdhci-omap 4809c000.mmc: Got CD GPIO
[    3.001870] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[    3.008513] sdhci-omap 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[    3.071003] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA
[    3.140824] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA
[    3.154076] ledtrig-cpu: registered to indicate activity on CPUs
[    3.167939] NET: Registered protocol family 10
[    3.173006] Segment Routing with IPv6
[    3.176717] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.184050] NET: Registered protocol family 17
[    3.188664] Key type dns_resolver registered
[    3.193101] omap_voltage_late_init: Voltage driver support not added
[    3.199523] Power Management for TI OMAP4+ devices.
[    3.204684] Registering SWP/SWPB emulation handler
[    3.218089] mmc0: host does not support reading read-only switch, assuming write-enable
[    3.226419] dmm 4e000000.dmm: workaround for errata i878 in use
[    3.232490] ti-iodelay 4844a000.padconf: Set reg 0x620 Delay(a: 600 g: 400), Elements(C=1 F=12)0x2902c
[    3.241904] ti-iodelay 4844a000.padconf: Set reg 0x628 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.250867] dmm 4e000000.dmm: initialized all PAT entries
[    3.256339] ti-iodelay 4844a000.padconf: Set reg 0x62c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.265270] ti-iodelay 4844a000.padconf: Set reg 0x634 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.274209] ti-iodelay 4844a000.padconf: Set reg 0x638 Delay(a: 30 g: 0), Elements(C=0 F=1)0x29001
[    3.274972] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.274974] [drm] No driver support for vblank timestamp query.
[    3.274998] [drm] Cannot find any crtc or sizes
[    3.296173] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[    3.296516] hctosys: unable to open rtc device (rtc0)
[    3.312702] ti-iodelay 4844a000.padconf: Set reg 0x640 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.312740] ALSA device list:
[    3.312743]   No soundcards found.
[    3.328007] ti-iodelay 4844a000.padconf: Set reg 0x644 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.328013] ti-iodelay 4844a000.padconf: Set reg 0x64c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.328019] ti-iodelay 4844a000.padconf: Set reg 0x650 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.328026] ti-iodelay 4844a000.padconf: Set reg 0x658 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.328031] ti-iodelay 4844a000.padconf: Set reg 0x65c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[    3.333900] mmc0: new ultra high speed SDR104 SDHC card at address aaaa
[    3.345892] mmcblk0: mmc0:aaaa SC16G 14.8 GiB 
[    3.368242]  mmcblk0: p1 p2
[    3.396193] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    3.404394] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    3.414801] devtmpfs: mounted
[    3.418627] Freeing unused kernel memory: 2048K
[    3.539775] systemd[1]: System time before build time, advancing clock.
[    3.562573] random: systemd: uninitialized urandom read (16 bytes read)
[    3.571842] random: systemd: uninitialized urandom read (16 bytes read)
[    3.581681] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[    3.600562] systemd[1]: Detected architecture arm.
[    4.064837] mmc1: new DDR MMC card at address 0001
[    4.069981] mmcblk1: mmc1:0001 R1J56L 13.8 GiB 
[    4.074736] mmcblk1boot0: mmc1:0001 R1J56L partition 1 16.0 MiB
[    4.080864] mmcblk1boot1: mmc1:0001 R1J56L partition 2 16.0 MiB
[    4.086996] mmcblk1rpmb: mmc1:0001 R1J56L partition 3 128 KiB
[    4.310844] [drm] Cannot find any crtc or sizes
[   33.754295] systemd[1]: Set hostname to <am57xx-evm>.
[   33.790329] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read)
[   33.791143] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read)
[   33.791293] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read)
[   63.832592] urandom_read: 1 callbacks suppressed
[   63.832597] random: systemd: uninitialized urandom read (16 bytes read)
[   63.844495] random: systemd: uninitialized urandom read (16 bytes read)
[   63.851855] random: systemd: uninitialized urandom read (16 bytes read)
[   64.149232] systemd[1]: Listening on Network Service Netlink Socket.
[   94.551135] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  124.631043] systemd[1]: Listening on Journal Socket (/dev/log).
[  154.710961] systemd[1]: Listening on Syslog Socket.
[  184.791013] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[  214.870903] systemd[1]: Reached target Swap.
[  244.951065] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  275.030902] systemd[1]: Reached target Paths.
[  305.115838] systemd[1]: Created slice User and Session Slice.
[  335.191041] systemd[1]: Listening on udev Control Socket.
[  365.270915] systemd[1]: Reached target Remote File Systems.
[  395.351563] systemd[1]: Created slice System Slice.

[ 4.105725] mmc1: new DDR MMC card at address 0001
[ 4.121292] mmcblk1: mmc1:0001 R1J56L 13.8 GiB
[ 4.126318] mmcblk1boot0: mmc1:0001 R1J56L partition 1 16.0 MiB
[ 4.132696] mmcblk1boot1: mmc1:0001 R1J56L partition 2 16.0 MiB
[ 4.138917] mmcblk1rpmb: mmc1:0001 R1J56L partition 3 128 KiB, chardev (244:0)
[ 4.392887] [drm] Cannot find any crtc or sizes
[ 34.396837] systemd[1]: Set hostname to <am57xx-evm>.
[ 64.831267] systemd[1]: Created slice System Slice.
[ 95.193675] systemd[1]: Created slice User and Session Slice.
[ 125.273168] systemd[1]: Listening on Network Service Netlink Socket.
[ 155.352934] systemd[1]: Reached target Swap.
[ 185.433106] systemd[1]: Listening on Journal Socket.
[ 215.513050] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 245.595469] systemd[1]: Mounting POSIX Message Queue File System...
[ 275.672978] systemd[1]: Reached target Remote File Systems.
[ 305.752966] systemd[1]: Reached target Slices.
[ 335.833792] systemd[1]: Created slice system-getty.slice.
[ 365.917955] systemd[1]: Listening on Syslog Socket.
[ 395.993035] systemd[1]: Listening on Journal Socket (/dev/log).
[ 426.085870] systemd[1]: Mounting Temporary Directory...
[ 456.168291] systemd[1]: Starting Journal Service...
[ 486.233812] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 516.315580] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 516.336817] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)