现在在使用AM5728进行DDR ECC设计时发现需要保证访问数据首地址32bit对齐(勘误表),另外在官网上看到的是AM5728是不支持ECC,AM5748是支持ECC的,所以我想问的是:
1)AM5748支持ECC是否不需要保证访问数据首地址32bit对齐,可以直接使用?
2)如果在AM5728硬件已经设计完成的情况下,是否可以在同一块硬件上用AM5748芯片直接替换AM5728,是否是pin to pin 兼容的?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1)AM5748默认CACHE打开的,会自动对齐,直接使用即可。
2,AM5748/5728 PIN TO PIN兼容的,可以直接替换。