This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

三相VIENNA PFC 控制板: F280049C controlCARD 评估模块 TMDSCNCD280049C无法连接到电脑



把控制板通过USB连接到电脑后,在CCS的Target Configuration中设置好connection和board or device,点击test connection,弹出的窗口显示
......
Scan tests: 2, skipped: 0, failed: 1
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 2
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 3
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 4
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 5
Some of the values were corrupted - 83.3 percent.

The JTAG DR Integrity scan-test has failed.

[End: Texas Instruments XDS100v2 USB Debug Probe_0]
即没有成功连接到目标板!

而且板上开关已按官网的信息指导Piccolo F280049 controlCARD Information Guide 设置好!

有人知道这是什么情况吗。怎么解决,急需解答,谢谢!