This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01589 这款开发板是否有TMS320C5517 DSP相应的sdk

Other Parts Discussed in Thread: TIDA-01589, TLV320ADC3101, TMS320C5517

TIDA-01589概述中提到

  • TLV320ADC3101 立体声 ADC,具有 92dBA SNR、0.003% THD,集成了 PGA、AGC 和 mini-DSP,用于实现抽取滤波功能
  • 功能强大的 TMS320C5517 DSP,用于实施各种音频处理算法,如:自适应频谱降噪 (ASNR) 和声学回声消除 (AEC),可处理回声尾部长达 128ms 的回声尾长

请问哪里可以获得以上功能的DSP参考算法呢。