KeyStone_common_CPU_init();
KeyStone_common_device_init();
//KeyStone_Exception_cfg(TRUE);
KeyStone_main_PLL_init(100, 10, 1);
Task_Handle task;
Error_Block eb;
int m;
unsigned char buf[11]={0x01,0x02,0x3,0x4,0x5,0x6,0x7,0x8,0x9,0xA,0xB};
printf("enter main()\n");
Error_init(&eb);
task = Task_create(taskFxn, NULL, &eb);
KeyStone_UART_config(115200,FALSE, UART_USE_CORE_TO_TX);
KeyStone_UART_write(buf, sizeof(buf), 0);
Hwi_Params hwi_uart;
Hwi_Handle myHwi;
CpIntc_dispatchPlug(149, (CpIntc_FuncPtr)UartIsr, 149 ,TRUE);
CpIntc_mapSysIntToHostInt(0, 149, 33);
CpIntc_enableHostInt(0,33);
CpIntc_enableSysInt(0, 149);
int eventId =CpIntc_getEventId(33);
Hwi_Params_init(&hwi_uart);
hwi_uart.arg =33;
hwi_uart.eventId =eventId;
hwi_uart.enableInt = TRUE;
myHwi = Hwi_create(12, CpIntc_dispatch, &hwi_uart, &eb);
Hwi_enableInterrupt(12); /* enable both interrupts */
主要代码如上,将外部事件149映射到主机中断33,然后是cpu中断12;自己无法找到问题所在,希望各位提供帮助。