目前我的工程是多核公用一个cfg,程序加载到多个核之后,出现main起始地址一样的情况,这样的话后面八个同时跑,出现各个段地址被相互改动就很有可能。我的问题是如何在cfg通过配置将八个核的各个段独立出来,这样互不干涉,才能使整个工程不回出现异常!请教一下各位,谢谢咯!(关于修改cmd文件的配置我知道怎么改,但是基于BIOS工程如何改,我不太清楚),在论坛上看到过类似的问题,但是没有解答,求指教,配置如下:
var Memory = xdc.useModule('xdc.runtime.Memory');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var HeapBuf = xdc.useModule('ti.sysbios.heaps.HeapBuf');
var Log = xdc.useModule('xdc.runtime.Log');
var Timer = xdc.useModule('ti.sysbios.hal.Timer');
var Mailbox = xdc.useModule('ti.sysbios.knl.Mailbox');
Program.stack = 0x10000;
/*
** Allow storing of task names. By default if you name a task with a friendly display name it will not be saved
** to conserve RAM. This must be set to true to allow it. We use friendly names on the Task List display.
*/
//Defaults.common$.namedInstance = true;
Task.common$.namedInstance = true;
var Clock = xdc.useModule ('ti.sysbios.knl.Clock');
/*
** Interface with IPC. Depending on the version of BIOS you are using the
** module name may have changed.
*/
/* Use this for pre BIOS 6.30 */
/* var Sem = xdc.useModule ('ti.sysbios.ipc.Semaphore'); */
/* Use this for BIOS 6.30 plus to get the IPC module */
var Sem = xdc.useModule ('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule ('ti.sysbios.hal.Hwi');
var Ecm = xdc.useModule ('ti.sysbios.family.c64p.EventCombiner');
var ti_sysbios_knl_Event = xdc.useModule('ti.sysbios.knl.Event');
/*
** Configure this to turn on the CPU Load Module for BIOS.
**
*/
/*
var Load = xdc.useModule('ti.sysbios.utils.Load');
Load.common$.diags_USER4 = Diags.ALWAYS_ON;
*/
var Diags = xdc.useModule('xdc.runtime.Diags');
/* Load the CSL package */
var Csl = xdc.useModule('ti.csl.Settings');
/* Load the CPPI package */
var Cppi = xdc.loadPackage('ti.drv.cppi');
/* Load the QMSS package */
var Qmss = xdc.loadPackage('ti.drv.qmss');
/* Load the PA package */
var Pa = xdc.useModule('ti.drv.pa.Settings');
/* Load the Platform/NDK Transport packages */
var PlatformLib = xdc.loadPackage('ti.platform.evmc6678l');
var NdkTransport = xdc.loadPackage('ti.transport.ndk');
/*
** Sets up the exception log so you can read it with ROV in CCS
*/
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Exc = xdc.useModule('ti.sysbios.family.c64p.Exception');
Exc.common$.logger = LoggerBuf.create();
Exc.enablePrint = true; /* prints exception details to the CCS console */
/*
** Give the Load module it's own LoggerBuf to make sure the
** events are not overwritten.
*/
/* var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.exitFlush = true;
loggerBufParams.numEntries = 64;
Load.common$.logger = LoggerBuf.create(loggerBufParams);
*/
/*
** Use this load to configure NDK 2.2 and above using RTSC. In previous versions of
** the NDK RTSC configuration was not supported and you should comment this out.
*/
var Global = xdc.useModule('ti.ndk.config.Global');
/*
** This allows the heart beat (poll function) to be created but does not generate the stack threads
**
** Look in the cdoc (help files) to see what CfgAddEntry items can be configured. We tell it NOT
** to create any stack threads (services) as we configure those ourselves in our Main Task
** thread hpdspuaStart.
*/
Global.enableCodeGeneration = false;
/* Define a variable to set the MAR mode for MSMCSRAM as all cacheable */
var Cache = xdc.useModule('ti.sysbios.family.c66.Cache');
//Cache.MAR224_255 = 0x0000000f;
var Startup = xdc.useModule('xdc.runtime.Startup');
var System = xdc.useModule('xdc.runtime.System');
/*
** Create a Heap.
*/
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = 0x300000;
heapMemParams.sectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
/* This is the default memory heap. */
Memory.defaultHeapInstance = Program.global.heap0;
Program.sectMap["sharedL2"] = "DDR3";
Program.sectMap["systemHeap"] = "DDR3";
Program.sectMap[".sysmem"] = "L2SRAM";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "L2SRAM";
Program.sectMap[".far"] = "L2SRAM";
Program.sectMap[".rodata"] = "L2SRAM";
Program.sectMap[".neardata"] = "L2SRAM";
Program.sectMap[".cppi"] = "DDR3";
Program.sectMap[".init_array"] = "DDR3";
Program.sectMap[".qmss"] = "DDR3";
Program.sectMap[".cinit"] = "L2SRAM";
Program.sectMap[".bss"] = "L2SRAM";
Program.sectMap[".const"] = "L2SRAM";
Program.sectMap[".text"] = "DDR3";
Program.sectMap[".code"] = "DDR3";
Program.sectMap[".switch"] = "L2SRAM";
Program.sectMap[".data"] = "L2SRAM";
Program.sectMap[".fardata"] = "DDR3";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "DDR3";
Program.sectMap[".vecs"] = "DDR3";
Program.sectMap["platform_lib"] = "DDR3";
Program.sectMap[".far:taskStackSection"] = "L2SRAM";
Program.sectMap[".stack"] = "L2SRAM";
Program.sectMap[".nimu_eth_ll2"] = "L2SRAM";
Program.sectMap[".resmgr_memregion"] = {loadSegment: "L2SRAM", loadAlign:128}; /* QMSS descriptors region */
Program.sectMap[".resmgr_handles"] = {loadSegment: "L2SRAM", loadAlign:16}; /* CPPI/QMSS/PA Handles */
Program.sectMap[".resmgr_pa"] = {loadSegment: "L2SRAM", loadAlign:8}; /* PA Memory */
Program.sectMap[".far:IMAGEDATA"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_OBJMEM"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_PACKETMEM"] = {loadSegment: "MSMCSRAM", loadAlign: 128};
Program.sectMap[".user_data_msmcsram"] = {loadSegment: "MSMCSRAM", loadAlign: 128};
/* Required if using System_printf to output on the console */
SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/********************************************************************************************************************
* Define hooks and static tasks that will always be running. *
********************************************************************************************************************/
/*
** Register an EVM Init handler with BIOS. This will initialize the hardware. BIOS calls before it starts.
**
** If yuo are debugging with CCS, then this function will execute as CCS loads it if the option in your
** Target Configuraiton file (.ccxml) has the option set to execute all code before Main. That is the
** default.
*/
Startup.lastFxns.$add('&EVM_init');
/*
** Create the stack Thread Task for our application.
*/
var tskNdkStackTest = Task.create("&StackTest");
tskNdkStackTest.stackSize = 0x2000;
tskNdkStackTest.priority = 5;
/*
** Create a Periodic task to handle all NDK polling functions.
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default and
** you do not need to do this.
*/
/*var prdNdkClkParams = new Clock.Params ();
prdNdkClkParams.period = 0x64;
prdNdkClkParams.startFlag = true;
Program.global.clockInst1 = Clock.create("&llTimerTick", 5, prdNdkClkParams);
*/
/*
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default, else
** register hooks so that the stack can track all Task creation
Task.common$.namedInstance = true;
Task.addHookSet ({ registerFxn: '&NDK_hookInit', createFxn: '&NDK_hookCreate', });
/* Enable BIOS Task Scheduler */
BIOS.taskEnabled = true;
/*
* Enable Event Groups here and registering of ISR for specific GEM INTC is done
* using EventCombiner_dispatchPlug() and Hwi_eventMap() APIs
*/
Ecm.eventGroupHwiNum[0] = 7;
Ecm.eventGroupHwiNum[1] = 8;
Ecm.eventGroupHwiNum[2] = 9;
Ecm.eventGroupHwiNum[3] = 10;
var hwi0Params = new Hwi.Params();
hwi0Params.instance.name = "hwi0";
hwi0Params.eventId = 20;
Program.global.hwi0 = Hwi.create(4, "&Isr_SrioDoorbell", hwi0Params);
var hwi1Params = new Hwi.Params();
hwi1Params.instance.name = "hwi1";
hwi1Params.eventId = 91;
Program.global.hwi1 = Hwi.create(5, "&Isr_Ipc", hwi1Params);