This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

最新SDK,内核无法得到nand flash分区信息,OOB size不够问题



AM437x

log如下

1.217199] GPIO line 151 (SelEMMCorNAND) hogged as output/low
[ 1.223812] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.229091] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.236796] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xdc
[ 1.243183] nand: Micron MT29F4G08ABADAWP
[ 1.247256] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.254928] Using OMAP_ECC_BCH16_CODE_HW ECC scheme
[ 1.259855] omap2-nand 8000000.nand: Not enough OOB bytes: required = 106, available=64
[ 1.267947] omap2-nand: probe of 8000000.nand failed with error -22

在uboot中,已经配置了OOB size为224,但这里还是64