This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
am335x处理器,linux-4.14.79,(ti-processor-sdk-linux-am335x-evm-05.02.00.10)
uvc标准摄像头,YUYV格式,320x240分辨率时工作正常,640x480时采集不到图像,跟踪驱动代码,看到以下信息:
uvcvideo: Marking buffer as bad (error bit set)
似乎是USB方面的问题。
如何解决这种问题?
我们自己做的板子,以前用的是linux-3.2.0内核,工作正常。现在想升级到4.14.79,才遇到这个问题。
跟踪了4.14.79的 drivers\media\usb\uvc 目录,部分信息:
uvcvideo: uvc_v4l2_open
uvcvideo: Resuming interface 0
uvcvideo: Resuming interface 1
uvcvideo: Trying format 0x56595559 (YUYV): 640x480.
uvcvideo: Using default frame interval 33333.3us (30.0 fps).
uvcvideo: uvc_v4l2_mmap
uvcvideo: uvc_v4l2_mmap
uvcvideo: uvc_v4l2_mmap
uvcvideo: uvc_v4l2_mmap
uvcvideo: Device requested 3072 B/frame bandwidth.
uvcvideo: Selecting alternate setting 7 (3072 B/frame bandwidth).
uvcvideo: Allocated 5 URB buffers of 32x3072 bytes each.
uvcvideo: uvc_v4l2_poll
uvc_video_decode_start, len: 2048, data[1]: 0c
uvc_video_decode_start, len: 2048, data[1]: 0c
uvc_video_decode_start, len: 3072, data[1]: 0c
uvc_video_decode_start, len: 2048, data[1]: 0c
uvc_video_decode_start, len: 2348, data[1]: 0c
uvc_video_decode_start, len: 2048, data[1]: 0c
uvc_video_decode_start, len: 3072, data[1]: 0c
uvc_video_decode_start, len: 2048, data[1]: 0c
uvc_video_decode_start, len: 3072, data[1]: 0c
uvc_video_decode_start, len: 1340, data[1]: 0c
uvc_video_decode_start, len: 3072, data[1]: 0c
uvc_video_decode_start, len: 3072, data[1]: 0c
uvc_video_decode_start, len: 1572, data[1]: 0c
uvc_video_decode_start, len: 12, data[1]: 4e
uvcvideo: Marking buffer as bad (error bit set).
uvcvideo: Frame complete (EOF found).
uvcvideo: EOF in empty payload.
uvc_video_decode_start, len: 12, data[1]: 0e
uvcvideo: Dropping payload (out of sync).
应用程序得不到图像数据,select timeout
v4l2-ctl -D
Driver Info (not using libv4l2):
Driver name : uvcvideo
Card type : FiberMicroscope
Bus info : usb-0000:00:06.0-2
Driver version: 4.10.17
Capabilities : 0x84200001
Video Capture
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04200001
Video Capture
Streaming
Extended Pix Format
放弃YUYV格式,采用MJPEG格式,采集图像正常。
谢谢各位关注。