This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320VC5509A的例程在CCS6.1.3中使用问题



您好,我是C5000系列的初学者,购买的5509A的开发板和100V3仿真器,CCS版本为6.1.3,电脑系统WIN10p 64位

在购买开发板时,客服提供了例程,但告知我只能在CCS3.3版本使用。我用CCS6.1.3 Import Legacy CCSV3.3 Project,出现报错,并且无法生成out文件。我没有看懂报错信息,自己摸索了两天还是不会更改。报错截图如下。

我有几个问题恳请您的指导:(1)这些工程确实没办法在CCS6.1.3用吗?还是我哪里操作不当?是因为我没有添加头文件和给头文件指定位置吗?如果需要添加头文件去哪里下载呢?(2)如果这些工程没办法在CCS6.1.3中直接使用,我可以新建一个工程对这些例程进行迁移嘛?如果迁移的话我需要怎么做,迁移哪些文件呢?(3)您可以提供给我一些直接在CCS6.1.3中直接使用的简单例程嘛?或者您告诉我去哪里下载,目前我在网上找到的都是低版本的工程。(4)像我这种新手有什么教程可以学习吗?我在网上一直没有找到有关DSP的教程,感觉这个对新手来说门槛有点高

非常期待您的回答!说了一大堆不是很有条理,给您添麻烦了!

/*
 *  Copyright 2003 by Texas Instruments Incorporated.
 *  All rights reserved. Property of Texas Instruments Incorporated.
 *  Restricted rights to use, duplicate or disclose this code are
 *  granted through contract.
 *  
 */
/* "@(#) DSP/BIOS 4.90.150 04-08-03 (barracuda-m02)" */
/******************************************************************************\
*           Copyright (C) 2000 Texas Instruments Incorporated.
*                           All Rights Reserved
*------------------------------------------------------------------------------
* MODULE NAME... WDTIM
* FILENAME...... wdt.c
* DATE CREATED.. Tu 11/03/2000 
* PROJECT....... Chip Support Library
* COMPONENT..... 
* PREREQUISITS.. 
*------------------------------------------------------------------------------
* HISTORY:
*   11/03/2000  (IM) Created
*  
*------------------------------------------------------------------------------
* DESCRIPTION:  
*   
* This is an example of the usage of WDTIM functions for 5509.
\*----------------------------------------------------------------------*/
#include <csl.h>
#include <csl_wdtim.h> 
#include <stdio.h>

int i, pscVal;
WDTIM_Config getConfig;
WDTIM_Config myConfig = {
     0x1000,          /* WDPRD */
     0x0000,          /* WDTCR */
     0x1000           /* WDTCR2 */
};


main()
{

    CSL_init();
  
#if (_WDTIM_SUPPORT)


    WDTIM_config(&myConfig);
    
    WDTIM_FSET(WDTCR, WDOUT, 1);           /* Connect to NMI */
    WDTIM_FSET(WDTCR, TDDR, 0xF);          /* Value to load PSC field */    
    WDTIM_FSET(WDTCR2, PREMD, 0);          /* Set direct mode */


        WDTIM_service();      /* enable watchdog */ 
          
    //for (i = 0; i < 100; i++)
        for (;;)
    {                     
        
        WDTIM_getConfig(&getConfig);  
        pscVal = WDTIM_FGET(WDTCR,PSC);

         printf("pscVal: %x, wdtcr: %x\n", 
                pscVal, getConfig.wdtcr);    
  
        
        /* write periodically to WDTIMER  - when this line is commented out,
           the watchdog times out, WDFLAG set to 1, indicating 
           that a Watchdog time-out occurred.*/ 
        WDTIM_service();         
    
    }           //end for loop
#endif
}



/******************************************************************************\
* End of wdt.c
\******************************************************************************/
6518.wdt.pjt