This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

K2G EVM development board failed to start from EMMC( K2G evm开发板 emmc启动不成功)



My K2G EVM development board failed to start through EMMC.

Operation steps:

1. After using SD card, EMMC is divided into FAT32 and ext3;

2. Compile the U boot with the default configuration of K2G ﹣ EVM ﹣ defconfig, and copy the MLO and u-boot.img files to the FAT32 partition

3. Turn the dial switch to EMMC start and turn on the power.

What are the wrong operations? What should I do to successfully start from EMMC? I hope to get some help. Thank you very much.

我的K2G evm开发板,通过emmc启动不成功。
操作步骤:
1、使用SD卡启动后,将emmc分区,分为Fat32和ext3格式的两个区;
2、使用k2g_evm_defconfig默认配置编译Uboot,将MLO和u-boot.img文件拷贝到Fat32分区
3、将拨码开关调到EMMC启动,接通电源。
哪些操作是错误的,我应该怎样做才能成功从EMMC启动,希望得到一些帮助,非常感谢。