This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D flash烧写报错“Loader: One or more sections of your program falls into a memory region that is not writable...”

Other Parts Discussed in Thread: CONTROLSUITE

问题描述:

进行的操作步骤如下:1、在电脑A上使用ccs6.0版本,已经成功实现LOAD程序进RAM正常运行;2、改烧flash(使用TI flash例程) 编译生成.out文件,而LOAD报错。错误信息如下:

C28xx_CPU2: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.

C28xx_CPU2: File Loader: Data verification failed at address 0x00080000 Please verify target memory and memory map.

C28xx_CPU2: GEL: File: H:\soft_install\controlsuite\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Dual\flash_programming\cpu02\ccs\CPU2_FLASH\flash_programming_cpu02.out: a data verification error occurred, file load failed.

3、在电脑B上使用ccs6.0烧写其他程序至该板件flash正常,后拷贝电脑1生成的TI flash烧写 例程 .out文件在电脑B中同样可以烧写成功。

(对比target configuration file 没有区别 仿真器与硬件一致)

现在不知道是哪里存在问题,怎么解决,

期待大家的回复,谢谢。