This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 两路独立高清编码的问题,第二路码流不对



您好 TIers:

接法是: VIP0_A  , 接了一路 1920x1080  30fps。

               VIP1_A  ,  接了一路 1280x1024  60fps。

----------------------------------------------------------------------------------------

软件配置了两个 IVAHD,各编码一路。  

LINK 是: CAP -->  OUT VPSS ---> IN VIDEO  ---> ENC  --->  BITS OUT  --->  HOST

请帮忙看看如下问题,谢谢。

有没有 两路独立高清编码 的 demo ?  谢谢

问题1:  dm8148 是否支持两路高清同时编码 ?

问题2:  第二个通道的码流获取的不对,size太小了,播放也没有图像。日志如下:

captureId= 536870945
ipcOutVpssId= 536870912
ipcInVideoId= 268435458
encId= 268435489
ipcBitsOutRTOSId= 268435480
ipcBitsInHLOSId= 805306394
69: MCFW : CPU Revision [ES2.1] !!!
[m3vpss ] 19980: CAPTURE: Create in progress !!!
[m3vpss ] CreateInst, numVipInst= 2
[m3vpss ] <CaptureLink_drvCreateInst> standard= 16
[m3vpss ] 20014: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!!
[m3vpss ] <CaptureLink_drvCreateInst> standard= 277
[m3vpss ] 20148: CAPTURE: VIP1 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!!
[m3video] 20285: IPC_IN_M3 : Create in progress !!!
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 58 (58)
[m3video] 20285: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3vpss ] UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
[m3video] 20286: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3vpss ] UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
[m3video] <Video IpcInM3Link_create> prevLinkId= 536870912, numQue= 4
[m3vpss ] UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
[m3video] i= 0, j= 0, width= 1920, height= 1080, scanFormat= 1
[m3vpss ] UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
[m3video] i= 0, j= 1, width= 1920, height= 1080, scanFormat= 1      //  怎么第二路还是 1920x1080, 我配置的是 1280x1024,请指点一下,谢谢
[m3video] 20289: IPC_IN_M3 : Create Done !!!
[m3video] 20289: ENCODE: Create in progress ... !!!
[m3vpss ] CAPTURE::HEAPID:0 USED:520
[m3vpss ] CAPTURE::HEAPID:4 USED:53913600
[m3vpss ] 20283: CAPTURE: Create Done !!!
[m3vpss ] 20284: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 20285: IPC_OUT_M3 : Create Done !!!
[m3video] <enc>inQueInfo.numCh= 2
[m3video] 20359: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1920, 1920) [PROGRESSIVE] [NON-TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[m3video] ENCLINK_H264:HEAPID:0 USED:13808
[m3video] ENCLINK_H264:HEAPID:3 USED:7176192
[m3video] 20399: ENCODE: Creating CH1 of 1920 x 1080, pitch = (1920, 1920) [PROGRESSIVE] [NON-TILED ], bitrate = 2000 Kbps, I-P Interval 1...

[host] IpcBitsInLink_tskMain:Entered[HOST]
ThreadName:IpcBitsInLink_tskMain_3000001a,ThreadID:303

[host] 532: IPC_BITS_IN : Create in progress !!!

[host] 532: IPC_BITS_IN : ListMPOpen start !!!

[host] 532: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_24] ...
534: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_24] ...

[host] 535: IPC_BITS_IN : ListMPOpen done !!!

[host] 536: IPC_BITS_IN : System_linkGetInfo done !!!

[host] 537: IPC_BITS_IN : Create Done !!!
[HOST]
ThreadName:IpcBitsInLink_periodicTaskFxn_3000001a,ThreadID:314
[m3vpss ] 20449: CAPTURE: Start in progress !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:7176192
[m3video] 20438: ENCODE: All CH Create ... DONE !!!
[m3video] ENCLINK:HEAPID:0 USED:25760
[m3video] ENCLINK:HEAPID:2 USED:12441600
[m3video] ENCLINK:HEAPID:3 USED:14352384
[m3video] 20439: ENCODE: Create ... DONE !!!
[m3video] 20440: IPC_BITS_OUT : Create in progress !!!
[m3video] 20442: IPC_BITS_OUT : Create Done !!!
[m3vpss ] 20548: CAPTURE: Enabled Time Stamping !!!
[m3vpss ] 20556: CAPTURE: Enabled Time Stamping !!!
[m3vpss ] 20564: CAPTURE: Start Done !!!
chid= 1, addr= 0x40c14080, size= 1377
chid= 1, addr= 0x40d11280, size= 165        // 1通道的码流不对
chid= 0, addr= 0x40e0e480, size= 45530
chid= 1, addr= 0x40f0b680, size= 70
chid= 1, addr= 0x41008880, size= 70
chid= 0, addr= 0x41105a80, size= 11017
chid= 1, addr= 0x41202c80, size= 75
chid= 1, addr= 0x412ffe80, size= 73
chid= 0, addr= 0x413fd080, size= 6462
chid= 1, addr= 0x414fa280, size= 70
chid= 1, addr= 0x415f7480, size= 70
chid= 0, addr= 0x416f4680, size= 7987
chid= 1, addr= 0x40c14080, size= 70
chid= 1, addr= 0x40d11280, size= 76
chid= 0, addr= 0x40e0e480, size= 361
chid= 1, addr= 0x40f0b680, size= 71
chid= 1, addr= 0x41008880, size= 71
chid= 0, addr= 0x41105a80, size= 18816
chid= 1, addr= 0x41202c80, size= 71

  • 你好,

    DM8148的编码性能大概是1080p60多一点,你现在的配置可能会超出编码能力。两路1080p30编码是可以的。

    请问你使用的是DVR RDK 4.01么?如果是,里面的DM8168 有一个HD Encode Card Use-case可以参考。