Hi:
在做AIF2苹果的过程中,阅读了AIF2 User Guide(文档编号为SPRUGV7D,下同)这个文档,有一些问题,不知各位专家能否帮我们解决一下,问题列表如下:
1在AIF2 user guide文档中,很多例子都是使用K28.7来举例,是否相应的K28.5在这些例子相同的场景中也能使用,还是TI在实现的时候,直接使用K28.7替代了K28.5?例如文档的4.4节,图4-11的说明?
2在AIF2 user guide 5.1.3中,第二段第一句说”CPRI implies that transmission should occur as soon as possible after reception”,请问这是否意味着如果使用CPRI协议的话,节点必须在接收完成后立刻进行发送,中间不能有间歇?
3 PhyT 10ms的帧长是否可变?在文档5.1.4节” Short Frame Mode”中提到了帧长可以从10ms减小到0.04ms,这是否意味着我们可以将做同步用的Phy帧设置的很短,而装载数据的无线帧设置的比较大?本节说,最短帧是32个WCDMA的chip,一个chip约为260ns,那么32个chip的时间是8320ns,不是0.04ms,请问最短帧帧长是0.04ms,还是8320ns?
4 在AIF2 user guide文档的149页,7.4.4.3中 frame_unsync_t 16bits,该位域是否只适用于OBSAI?
5 Pi和Delta的概念只在OBSAI中有,在CPRI中没有,请问TI在AIF2实现的时候,是否这种机制在两种协议下都有效?
6 文档中说AIF2实现了CPRI4.0协议,而CPRI4.0协议只能最高支持5X,在AIF2文档中却说CPRI协议可以支持8X,请问这是怎么做到的?
7 在AIF2 User Guide的5.2.4节中有如下的描述” Software writes the initial value of AT timers”,请问这个值软件如何确定,该写多少?